SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Table 30-5 lists the resets used in the VCP1 and VCP2 modules.
Type | Name | Source | Description |
---|---|---|---|
Hardware | VCP1_RST VCP2_RST | PRCM | Global Reset |
Software | VCP_SYSCONFIG[0] RESET_DONE | Internal | Reset from the idle command, reset is complete when its value is 1 |
This section covers the reset feature of the VCP1 and VCP2 modules.
The VCP_SYSCONFIG[0] RESET_DONE bit shows the status of the reset from the idle command. It indicates that the reset is complete when its value is 1. Software must ensure that the reset completes before doing VCP operations.
The behavior of software reset and hardware reset is the same, except that the software reset bit resets this module without affecting the whole device reset core domain.