SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Bits 15-0 are the number of lines to be transferred in the current channel. This is ignored for outbound transfers as the client will provide the line length with the end of frame signal on the client interface. The maximum supported transfer size is currently 2048.