SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
The CPSW_3G software reset register (CPSW_SOFT_RESET), CPSW_3GSS software reset register (WR_SOFT_RESET) and the three submodule software reset registers enable the CPSW_3GSS to be reset by software.
There are three CPSW_3G submodules that contain software reset registers (CPGMAC_SL1, CPGMAC_SL2 (SL_SOFT_RESET), and CPDMA (CPDMA_SOFT_RESET)). Each of the three submodules may be individually commanded to be reset by software.
For the CPDMA, the reset state is entered at packet boundaries, at which time the CPDMA reset occurs. The CPGMAC_SL soft reset is immediate. Submodule reset status is determined by reading or polling the submodule reset bit. If the submodule reset bit is read as a one, then the reset process has not yet completed. The submodule soft reset process could take up to 2ms each. The reset has completed if the submodule reset bit is read as a zero.
After all three submodules (in any order) have been reset and a read of each submodule reset bit indicates that the reset process is complete, the CPSW_3G software reset register bit may be written to complete the CPSW_3G module software reset operation. The CPSW_3G software reset bit controls the reset of the FIFO's, the statistics submodule, and the address lookup engine (ALE). The CPSW_3G software reset is immediate and will be indicated by reading a zero from the soft reset bit.
The CPSW_3GSS software reset bit controls the reset of the INT, REGS, and CPPI. The CPSW_3GSS software reset is immediate and will be indicated by reading a zero from the soft reset bit.