SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
The L3_MAIN VBUF address should be mapped to a valid CBUF region. If this address is mapped to none of the configured CBUF regions, then the OCM controller generates a virtual address error or out of range CBUF address error event. It is possible both virtual address error and out of range CBUF address error to be generated. The L3_MAIN VBUF address caused these two events can be read through the LAST_ILLEGAL_OCMC_ADDR[31:0] ADDR bit field.
Virtual address error is generated when the L3_MAIN VBUF address is lower than the virtual frame start address. This is indicated by asserting the INTR0_STATUS_RAW_SET[4] CBUF_VIRTUAL_ADDR_ERR_FOUND/INTR1_STATUS_RAW_SET[4] CBUF_VIRTUAL_ADDR_ERR_FOUND bit.
The out of range CBUF address error is generated when the L3_MAIN VBUF address is greater than the virtual frame end address. This error is an indication of an unexpected change in the frame size or a long frame and should be handled immediately to prevent further memory corruption. The out of range CBUF address error can be caused when performing write or read access. The out of range CBUF write address error is indicated by the STATUS_CBUF_WR_OUT_OF_RANGE_ERR[11:0] CBUF_ERR bit field. The out of range CBUF read address error is indicated by the STATUS_CBUF_RD_OUT_OF_RANGE_ERROR[11:0] CBUF_ERR bit field. Each bit in these registers is associated only with one CBUF. Bit 0 corresponds to CBUF_0, bit 1 corresponds to CBUF_1 and so on. A value of 0x1 for each bit means that there is an error (CBUF address is out of CBUF range) for the corresponding CBUF. Writing 0x1 for each bit clears the status.
The INTR0_STATUS_RAW_SET[5] CBUF_WR_OUT_OF_RANGE_ERR_FOUND/INTR1_STATUS_RAW_SET[5] CBUF_WR_OUT_OF_RANGE_ERR_FOUND bit is asserted if at least one of the bits in the STATUS_CBUF_WR_OUT_OF_RANGE_ERR[11:0] CBUF_ERR bit field is set to 0x1.
The INTR0_STATUS_RAW_SET[8] CBUF_READ_OUT_OF_RANGE_ERR_FOUND/INTR1_STATUS_RAW_SET[8] CBUF_READ_OUT_OF_RANGE_ERR_FOUND bit is asserted if at least one of the bits in the STATUS_CBUF_RD_OUT_OF_RANGE_ERROR[11:0] CBUF_ERR bit field is set to 0x1.