SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Suppose an external device is sending two dissimilar sources in Line Multiplex mode. One narrower source has X pixels per line. The wider source has 2X pixels per line.
The Meta Data has provisions for the external device to split a line. The Beginning of Line (BOL) and End of Line (EOL) flags tag a split line as described in Table 9-14.
BOL | EOL | Function |
---|---|---|
0 | 0 | Undefined |
0 | 1 | Line Segment is the second half of a line |
1 | 0 | Line Segment is the first half of a line |
1 | 1 | Line has not been segmented into two. |