SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
A Sync on LM Timer descriptor sets a value from the current timer position to wait. The LM timer is a free running counter at the LM processing clock. The Timer Value in the descriptor is added to the value of the timer at the time the descriptor is received and the list will stall for this many cycles before it becomes active again.