SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Next Descriptor Pointer
The 32-bit word aligned memory address of the next buffer descriptor in the RX queue. This is the mechanism used to reference the next buffer descriptor from the current buffer descriptor. If the value of this pointer is zero then the current buffer is the last buffer in the queue. The host sets the Next_Descriptor_Pointer.