SPRUI33H November 2015 – June 2024 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
Table 3-403 lists the memory-mapped registers for the DCSM_BANK1_Z2_OTP registers. All register offset addresses not listed in Table 3-403 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Write Protection | Section |
---|---|---|---|---|
0h | B1_Z2OTP_LINKPOINTER1 | Zone 2 Link Pointer1 in Z2 OTP for flash BANK1 | Go | |
4h | B1_Z2OTP_LINKPOINTER2 | Zone 2 Link Pointer2 in Z2 OTP for flash BANK1 | Go | |
8h | B1_Z2OTP_LINKPOINTER3 | Zone 2 Link Pointer3 in Z2 OTP for flash BANK1 | Go |
Complex bit access types are encoded to fit into small table cells. Table 3-404 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
Reset or Default Value | ||
-n | Value after reset or the default value | |
Register Array Variables | ||
i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. |
B1_Z2OTP_LINKPOINTER1 is shown in Figure 3-357 and described in Table 3-405.
Return to the Summary Table.
Zone 2 Link Pointer1 in Z2 OTP for flash BANK1
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
B1_Z2OTP_LINKPOINTER1 | |||||||||||||||||||||||||||||||
R-FFFFFFFFh | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | B1_Z2OTP_LINKPOINTER1 | R | FFFFFFFFh | Zone2 Link Pointer 1 location in USER OTP of Flash BANK1. Reset type: SYSRSn |
B1_Z2OTP_LINKPOINTER2 is shown in Figure 3-358 and described in Table 3-406.
Return to the Summary Table.
Zone 2 Link Pointer2 in Z2 OTP for flash BANK1
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
B1_Z2OTP_LINKPOINTER2 | |||||||||||||||||||||||||||||||
R-FFFFFFFFh | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | B1_Z2OTP_LINKPOINTER2 | R | FFFFFFFFh | Zone2 Link Pointer 2 location in USER OTP of Flash BANK1. Reset type: SYSRSn |
B1_Z2OTP_LINKPOINTER3 is shown in Figure 3-359 and described in Table 3-407.
Return to the Summary Table.
Zone 2 Link Pointer3 in Z2 OTP for flash BANK1
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
B1_Z2OTP_LINKPOINTER3 | |||||||||||||||||||||||||||||||
R-FFFFFFFFh | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | B1_Z2OTP_LINKPOINTER3 | R | FFFFFFFFh | Zone2 Link Pointer 3 location in USER OTP of Flash BANK1. Reset type: SYSRSn |