SPRUI33H November 2015 – June 2024 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
Table 3-346 lists the memory-mapped registers for the FLASH_ECC_REGS registers. All register offset addresses not listed in Table 3-346 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Write Protection | Section |
---|---|---|---|---|
0h | ECC_ENABLE | ECC Enable | EALLOW | Go |
2h | SINGLE_ERR_ADDR_LOW | Single Error Address Low | EALLOW | Go |
4h | SINGLE_ERR_ADDR_HIGH | Single Error Address High | EALLOW | Go |
6h | UNC_ERR_ADDR_LOW | Uncorrectable Error Address Low | EALLOW | Go |
8h | UNC_ERR_ADDR_HIGH | Uncorrectable Error Address High | EALLOW | Go |
Ah | ERR_STATUS | Error Status | EALLOW | Go |
Ch | ERR_POS | Error Position | EALLOW | Go |
Eh | ERR_STATUS_CLR | Error Status Clear | EALLOW | Go |
10h | ERR_CNT | Error Control | EALLOW | Go |
12h | ERR_THRESHOLD | Error Threshold | EALLOW | Go |
14h | ERR_INTFLG | Error Interrupt Flag | EALLOW | Go |
16h | ERR_INTCLR | Error Interrupt Flag Clear | EALLOW | Go |
18h | FDATAH_TEST | Data High Test | EALLOW | Go |
1Ah | FDATAL_TEST | Data Low Test | EALLOW | Go |
1Ch | FADDR_TEST | ECC Test Address | EALLOW | Go |
1Eh | FECC_TEST | ECC Test Address | EALLOW | Go |
20h | FECC_CTRL | ECC Control | EALLOW | Go |
22h | FOUTH_TEST | Test Data Out High | EALLOW | Go |
24h | FOUTL_TEST | Test Data Out Low | EALLOW | Go |
26h | FECC_STATUS | ECC Status | EALLOW | Go |
Complex bit access types are encoded to fit into small table cells. Table 3-347 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
R-0 | R -0 | Read Returns 0s |
Write Type | ||
W | W | Write |
W1S | W 1S | Write 1 to set |
Reset or Default Value | ||
-n | Value after reset or the default value | |
Register Array Variables | ||
i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. |
ECC_ENABLE is shown in Figure 3-310 and described in Table 3-348.
Return to the Summary Table.
ECC Enable
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0h | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | ENABLE | ||||||||||||||
R-0h | R/W-Ah | ||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-4 | RESERVED | R | 0h | Reserved |
3-0 | ENABLE | R/W | Ah | ECC enable. A value of 0xA would enable ECC. Any other value would disable ECC. Reset type: SYSRSn |
SINGLE_ERR_ADDR_LOW is shown in Figure 3-311 and described in Table 3-349.
Return to the Summary Table.
Single Error Address Low
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
ERR_ADDR_L | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ERR_ADDR_L | R/W | 0h | 64-bit aligned address at which a single bit error occurred in the lower 64-bits of a 128-bit aligned memory. Reset type: SYSRSn |
SINGLE_ERR_ADDR_HIGH is shown in Figure 3-312 and described in Table 3-350.
Return to the Summary Table.
Single Error Address High
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
ERR_ADDR_H | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | ERR_ADDR_H | R/W | 0h | 64-bit aligned address at which a single bit error occurred in the upper 64-bits of a 128-bit aligned memory. Reset type: SYSRSn |
UNC_ERR_ADDR_LOW is shown in Figure 3-313 and described in Table 3-351.
Return to the Summary Table.
Uncorrectable Error Address Low
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
UNC_ERR_ADDR_L | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | UNC_ERR_ADDR_L | R/W | 0h | 64-bit aligned address at which an uncorrectable error occurred in the lower 64-bits of a 128-bit aligned memory. Reset type: SYSRSn |
UNC_ERR_ADDR_HIGH is shown in Figure 3-314 and described in Table 3-352.
Return to the Summary Table.
Uncorrectable Error Address High
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
UNC_ERR_ADDR_H | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | UNC_ERR_ADDR_H | R/W | 0h | 64-bit aligned address at which an uncorrectable error occurred in the upper 64-bits of a 128-bit aligned memory. Reset type: SYSRSn |
ERR_STATUS is shown in Figure 3-315 and described in Table 3-353.
Return to the Summary Table.
Error Status
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | UNC_ERR_H | FAIL_1_H | FAIL_0_H | ||||
R-0h | R-0h | R-0h | R-0h | ||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | UNC_ERR_L | FAIL_1_L | FAIL_0_L | ||||
R-0h | R-0h | R-0h | R-0h | ||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-19 | RESERVED | R | 0h | Reserved |
18 | UNC_ERR_H | R | 0h | Uncorrectable error. A value of 1 indicates that an un-correctable error occurred in upper 64bits of a 128-bit aligned address. Cleared by writing a 1 to UNC_ERR_H_CLR bit of ERR_STATUS_CLR register. Reset type: SYSRSn |
17 | FAIL_1_H | R | 0h | Fail on 1. 0 Fail on 1 single bit error did not occur in upper 64bits of a 128-bit aligned address. 1 A value of 1 would indicate that a single bit error occurred in upper 64bits of a 128-bit aligned address and the corrected value was 1. Cleared by writing a 1 to FAIL_1_H_CLR bit of ERR_STATUS_CLR register. Note: This bit is updated on every flash access which results in a single bit error, So, in case of multiple single bit error, the status would correspond to the last error which occured. Reset type: SYSRSn |
16 | FAIL_0_H | R | 0h | Fail on 0. 0 Fail on 0 single bit error did not occur in upper 64bits of a 128-bit aligned address. 1 A value of 1 would indicate that a single bit error occurred in upper 64bits of a 128-bit aligned address and the corrected value was 0. Cleared by writing a 1 to FAIL_0_H_CLR bit of ERR_STATUS_CLR register. Note: This bit is updated on every flash access which results in a single bit error, So, in case of multiple single bit error, the status would correspond to the last error which occurred. Reset type: SYSRSn |
15-3 | RESERVED | R | 0h | Reserved |
2 | UNC_ERR_L | R | 0h | Uncorrectable error. A value of 1 indicates that an un-correctable error occurred in lower 64bits of a 128-bit aligned address. Cleared by writing a 1 to UNC_ERR_L_CLR bit of ERR_STATUS_CLR register. Reset type: SYSRSn |
1 | FAIL_1_L | R | 0h | Fail on 1. 0 Fail on 1 single bit error did not occur in lower 64bits of a 128-bit aligned address. 1 A value of 1 would indicate that a single bit error occurred in lower 64bits of a 128-bit aligned address and the corrected value was 1. Cleared by writing a 1 to FAIL_1_L_CLR bit of ERR_STATUS_CLR register. Note: This bit is updated on every flash access which results in a single bit error, So, in case of multiple single bit error, the status would correspond to the last error which occured. Reset type: SYSRSn |
0 | FAIL_0_L | R | 0h | Fail on 0. 0 Fail on 0 single bit error did not occur in lower 64bits of a 128-bit aligned address. 1 Would indicate that a single bit error occurred in lower 64bits of a 128-bit aligned address and the corrected value was 0. Cleared by writing a 1 to FAIL_0_L_CLR bit of ERR_STATUS_CLR register. Note: This bit is updated on every flash access which results in a single bit error, So, in case of multiple single bit error, the status would correspond to the last error which occured. Reset type: SYSRSn |
ERR_POS is shown in Figure 3-316 and described in Table 3-354.
Return to the Summary Table.
Error Position
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | ERR_TYPE_H | ||||||
R-0h | R-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | ERR_POS_H | ||||||
R-0h | R-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | ERR_TYPE_L | ||||||
R-0h | R-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | ERR_POS_L | ||||||
R-0h | R-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | RESERVED | R | 0h | Reserved |
24 | ERR_TYPE_H | R | 0h | Error type 0 Indicates that a single bit error occured in upper 64 data bits of a 128-bit aligned address. 1 Indicates that a single bit error occured in ECC check bits of upper 64bits of a 128-bit aligned address. Reset type: SYSRSn |
23-22 | RESERVED | R | 0h | Reserved |
21-16 | ERR_POS_H | R | 0h | Error position. Bit position of the single bit error in upper 64bits of a 128-bit aligned address. The position is interpreted depending on whether the ERR_TYPE bit indicates a check bit or a data bit. If ERR_TYPE indicates a check bit error, the error position could range from 0 to 7, else it could range from 0 to 63. Reset type: SYSRSn |
15-9 | RESERVED | R | 0h | Reserved |
8 | ERR_TYPE_L | R | 0h | Error type 0 Indicates that a single bit error occured in lower 64 data bits of a 128-bit aligned address. 1 Indicates that a single bit error occured in ECC check bits of lower 64bits of a 128-bit aligned address. Reset type: SYSRSn |
7-6 | RESERVED | R | 0h | Reserved |
5-0 | ERR_POS_L | R | 0h | Error position. Bit position of the single bit error in lower 64bits of a 128-bit aligned address. The position is interpreted depending on whether the ERR_TYPE bit indicates a check bit or a data bit. If ERR_TYPE indicates a check bit error, the error position could range from 0 to 7, else it could range from 0 to 63. Reset type: SYSRSn |
ERR_STATUS_CLR is shown in Figure 3-317 and described in Table 3-355.
Return to the Summary Table.
Error Status Clear
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | UNC_ERR_H_CLR | FAIL_1_H_CLR | FAIL_0_H_CLR | ||||
R-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | ||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | UNC_ERR_L_CLR | FAIL_1_L_CLR | FAIL_0_L_CLR | ||||
R-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | ||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-19 | RESERVED | R | 0h | Reserved |
18 | UNC_ERR_H_CLR | R-0/W1S | 0h | Uncorrectable error clear. Writing a 1 to this bit will clear the UNC_ERR_H bit of ERR_STATUS register. Writes of 0 have no effect. Read returns 0. Reset type: SYSRSn |
17 | FAIL_1_H_CLR | R-0/W1S | 0h | Fail on 1 clear. Writing a 1 to this bit will clear the FAIL_1_H bit of ERR_STATUS register. Writes of 0 have no effect. Read returns 0. Reset type: SYSRSn |
16 | FAIL_0_H_CLR | R-0/W1S | 0h | Fail on 0 clear. Writing a 1 to this bit will clear the FAIL_0_H bit of ERR_STATUS register. Writes of 0 have no effect. Read returns 0. Reset type: SYSRSn |
15-3 | RESERVED | R | 0h | Reserved |
2 | UNC_ERR_L_CLR | R-0/W1S | 0h | Uncorrectable error clear. Writing a 1 to this bit will clear the UNC_ERR_L bit of ERR_STATUS register. Writes of 0 have no effect. Read returns 0. Reset type: SYSRSn |
1 | FAIL_1_L_CLR | R-0/W1S | 0h | Fail on 1 clear. Writing a 1 to this bit will clear the FAIL_1_L bit of ERR_STATUS register. Writes of 0 have no effect. Read returns 0. Reset type: SYSRSn |
0 | FAIL_0_L_CLR | R-0/W1S | 0h | Fail on 0 clear. Writing a 1 to this bit will clear the FAIL_0_L bit of ERR_STATUS register. Writes of 0 have no effect. Read returns 0. Reset type: SYSRSn |
ERR_CNT is shown in Figure 3-318 and described in Table 3-356.
Return to the Summary Table.
Error Control
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | ERR_CNT | ||||||||||||||||||||||||||||||
R-0h | R/W-0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-0 | ERR_CNT | R/W | 0h | Single bit error count. This counter increments with every single bit ECC error occurrence. Upon reaching the threshold value counter stops counting on single bit errors. ERR_CNT can be cleared (irrespective of whether threshold is met or not) using 'Single Err Int Clear' bit. This is applicable for ECC logic test mode and normal operational mode. Reset type: SYSRSn |
ERR_THRESHOLD is shown in Figure 3-319 and described in Table 3-357.
Return to the Summary Table.
Error Threshold
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | ERR_THRESHOLD | ||||||||||||||||||||||||||||||
R-0h | R/W-0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-0 | ERR_THRESHOLD | R/W | 0h | Single bit error threshold. Sets the threshold for single bit errors. When the ERR_CNT value equals the THRESHOLD value and a single bit error occurs, SINGLE_ERR_INT flag is set, and an interrupt is fired. Reset type: SYSRSn |
ERR_INTFLG is shown in Figure 3-320 and described in Table 3-358.
Return to the Summary Table.
Error Interrupt Flag
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | UNC_ERR_INTFLG | SINGLE_ERR_INTFLG | |||||
R-0h | R-0h | R-0h | |||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-2 | RESERVED | R | 0h | Reserved |
1 | UNC_ERR_INTFLG | R | 0h | Uncorrectable bit error interrupt flag. When a Un-correctable error occurs, this bit is set and the UNC_ERR_INT interrupt is fired. When UNC_ERR_INTCLR bit of ERR_INTCLR register is written a value of 1 this bit is cleared. Reset type: SYSRSn |
0 | SINGLE_ERR_INTFLG | R | 0h | Single bit error interrupt flag. When the ERR_CNT value equals the ERR_THRESHOLD value and a single bit error occurs then SINGLE_ERR_INT flag is set and SINGLE_ERR_INT interrupt is fired. When SINGLE_ERR_INTCLR bit of ERR_INTCLR register is written a value of 1 this bit is cleared. Reset type: SYSRSn |
ERR_INTCLR is shown in Figure 3-321 and described in Table 3-359.
Return to the Summary Table.
Error Interrupt Flag Clear
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | UNC_ERR_INTCLR | SINGLE_ERR_INTCLR | |||||
R-0h | R-0/W1S-0h | R-0/W1S-0h | |||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-2 | RESERVED | R | 0h | Reserved |
1 | UNC_ERR_INTCLR | R-0/W1S | 0h | Uncorrectable bit error interrupt flag clear. Writing a 1 to this bit will clear UNC_ERR_INT_FLG. Writes of 0 have no effect. Reset type: SYSRSn |
0 | SINGLE_ERR_INTCLR | R-0/W1S | 0h | Single bit error interrupt flag clear. Writing a 1 to this bit will clear SINGLE_ERR_INT_FLG. Writes of 0 have no effect. Reset type: SYSRSn |
FDATAH_TEST is shown in Figure 3-322 and described in Table 3-360.
Return to the Summary Table.
Data High Test
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
FDATAH | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | FDATAH | R/W | 0h | High double word of selected 64-bit data. User-configurable bits 63:32 of the selected data block in ECC test mode. Reset type: SYSRSn |
FDATAL_TEST is shown in Figure 3-323 and described in Table 3-361.
Return to the Summary Table.
Data Low Test
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
FDATAL | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | FDATAL | R/W | 0h | Low double word of selected 64-bit data. User-configurable bits 31:0 of the selected data block in ECC test mode. Reset type: SYSRSn |
FADDR_TEST is shown in Figure 3-324 and described in Table 3-362.
Return to the Summary Table.
ECC Test Address
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | ADDRH | ||||||||||||||
R-0h | R/W-0h | ||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
ADDRL | RESERVED | ||||||||||||||
R/W-0h | R-0h | ||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-22 | RESERVED | R | 0h | Reserved |
21-16 | ADDRH | R/W | 0h | Address for selected 64-bit data. User-configurable address bits of the selected data in ECC test mode. Left-shift the address by one bit (to provide byte address) and ignore the three least significant bits of the address and write the bits 21:16 in remaining address bits in this field. Reset type: SYSRSn |
15-3 | ADDRL | R/W | 0h | Address for selected 64-bit data. User-configurable address bits of the selected data in ECC test mode. Left-shift the address by one bit (to provide byte address) and ignore the three least significant bits of the address and write the bits 15:3 in remaining address bits in this field. Reset type: SYSRSn |
2-0 | RESERVED | R | 0h | Reserved |
FECC_TEST is shown in Figure 3-325 and described in Table 3-363.
Return to the Summary Table.
ECC Test Address
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | RESERVED | ECC | |||||||||||||||||||||||||||||
R-0h | R-0h | R/W-0h | |||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-8 | RESERVED | R | 0h | Reserved |
7-0 | ECC | R/W | 0h | 8-bit ECC for selected 64-bit data. User-configurable ECC bits of the selected 64-bit data block in ECC test mode. Reset type: SYSRSn |
FECC_CTRL is shown in Figure 3-326 and described in Table 3-364.
Return to the Summary Table.
ECC Control
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DO_ECC_CALC | ECC_SELECT | ECC_TEST_EN | ||||
R-0h | R-0/W1S-0h | R/W-0h | R/W-0h | ||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-3 | RESERVED | R | 0h | Reserved |
2 | DO_ECC_CALC | R-0/W1S | 0h | Enable ECC calculation. ECC logic will calculate ECC in one cycle for the data and address written in ECC test registers when ECC test logic is enabled by setting ECC_TEST_EN. Reset type: SYSRSn |
1 | ECC_SELECT | R/W | 0h | ECC block select. 0 Selects the ECC block on bits [63:0] of bank data. 1 Selects the ECC block on bits [127:64] of bank data. Reset type: SYSRSn |
0 | ECC_TEST_EN | R/W | 0h | ECC test mode enable. 0 ECC test mode disabled 1 ECC test mode enabled Reset type: SYSRSn |
FOUTH_TEST is shown in Figure 3-327 and described in Table 3-365.
Return to the Summary Table.
Test Data Out High
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATAOUTH | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | DATAOUTH | R | 0h | High double word test data out. Holds bits 63:32 of the data out of the selected ECC block. Reset type: SYSRSn |
FOUTL_TEST is shown in Figure 3-328 and described in Table 3-366.
Return to the Summary Table.
Test Data Out Low
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATAOUTL | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | DATAOUTL | R | 0h | Low double word test data out. Holds bits 31:0 of the data out of the selected ECC block. Reset type: SYSRSn |
FECC_STATUS is shown in Figure 3-329 and described in Table 3-367.
Return to the Summary Table.
ECC Status
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | ERR_TYPE | ||||||
R-0h | R-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DATA_ERR_POS | UNC_ERR | SINGLE_ERR | |||||
R-0h | R-0h | R-0h | |||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-9 | RESERVED | R | 0h | Reserved |
8 | ERR_TYPE | R | 0h | Test mode ECC single bit error indicator. When 1, indicates that the single bit error is in check bits. When 0, indicates that the single bit error is in data bits (If SINGLE_ERR field is also set). Reset type: SYSRSn |
7-2 | DATA_ERR_POS | R | 0h | Test mode single bit error position. Holds the bit position where the single bit error occurred. The position is interpreted depending on whether the CHK_ERR bit indicates a check bit or a data bit. If CHK_ERR indicates a check bit error, the error position could range from 0 to 7, or it could range from 0 to 63. Reset type: SYSRSn |
1 | UNC_ERR | R | 0h | Test mode ECC double bit error. When 1 indicates that the ECC test resulted in an uncorrectable bit error. Reset type: SYSRSn |
0 | SINGLE_ERR | R | 0h | Test mode ECC single bit error. When 1 indicates that the ECC test resulted in a single bit error. Reset type: SYSRSn |