SPRUI33H November 2015 – June 2024 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
FILE: fsi_ex13_single_line_delay_select_tx.c
In order to understand this example better and visualize the results please refer to: Fast Serial Interface (FSI) Skew Compensation
Companion: fsi_single_line_delay_select_rx This example configures the FSI module to transmit pings at single data rate (using RXD0). Run the C28x device with this application first then run the core with the fsi_single_line_delay_select_rx application. This example must be used with fsi_single_line_delay_select_rx
In fsi_single_line_delay_select_rx (RX Device) example, the FSI module is configured to listen for a ping at single data rate (using RXD0). The software tests whether the ping sent from the TX device is correctly received against all combinations of delay elements activated. RXD0: 0-31 delay elements activated RXCLK: 0-31 delay elements activated The software stores the status of the ping received (fail/pass) for each of the 32x32 combinations of the delay line elements. This result can be graphed using the FSI Skew Compensation Utility.
External Connections
For FSI external connection, make below GPIO settings in example code.
ControlCard FSI Header GPIOs:
LaunchPad FSI Header GPIOs: