SPRUIC4D January 2017 – June 2022
The controlCARD, by default, assumes the F280049C internal VREG will be used to generate the 1.2-V power supply required by the MCU. The controlCARD enables the user to use the internal DC/DC converter capabilities, with some soldering.
To enable the internal DC/DC converter:
Functionally, the F280049C powers up the 1.2-V power rail using the internal VREG, then requires software to change from the VREG to the DC/DC. See the F28004x Technical Reference Manual for more details.