SPRUID8D September 2020 – January 2022 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
Interrupts from external sources can be provided to the device using GPIO pins with help of XINT module. The module allows configuring the GPIOs to be selected as interrupt sources. The polarity of the interrupts can also be configured with this module.
The following tests can be applied as diagnostics for this module (to provide diagnostic coverage on a specific function):