SPRUID8D September 2020 – January 2022 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
The CLA_STL, implements the CLA2 - Software Test of CLA. Similar to the C28x_STL the CLA_STL’s startup tests are also destructive in nature and should be run during startup operations. The CLA_STL’s run time tests comprise the bulk of the tests designed to run in conjunction with the host application. The CLA host application must allocate the time and space for the run time tests. The CPU must run both the CLA_STL POST and PEST tests for maximum diagnostic coverage. See the SPS delivered with the CSP for the exact DC requirements applicable to the CLA_STL.
The system integrator must consult the CLA_STL user guides and understand all aspects of integrating the library into the host application.