SPRUID8D September 2020 – January 2022 TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1
The enhanced Peripheral Interrupt Expander (ePIE) module is used to interface peripheral interrupts to the C28x CPU. It provides configurable masking on a per interrupt basis. The PIE module includes a local SRAM that is used to hold the address of the interrupt handler per interrupt.
The following tests can be applied as diagnostics for this module (to provide diagnostic coverage on a specific function):
The following tests can be applied as a test-for-diagnostic on this module: