SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The CLB Input X-BAR is architecturally identical to the Input X-BAR. The only difference is the destination for each INPUTx. The destination for each INPUTx is only the CLB Tiles as shown in Table 17-2. This allows for GPIOs to be accessed by the CLB tiles without using the combination of Input X-BAR and CLB X-BAR.
INPUT | CLB |
---|---|
1 | Yes |
2 | Yes |
3 | Yes |
4 | Yes |
5 | Yes |
6 | Yes |
7 | Yes |
8 | Yes |
9 | Yes |
10 | Yes |
11 | Yes |
12 | Yes |
13 | Yes |
14 | Yes |
15 | Yes |
16 | Yes |