SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Table 8-23 lists the memory-mapped registers for the CLA_ONLY_REGS registers. All register offset addresses not listed in Table 8-23 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Write Protection | Section |
---|---|---|---|---|
80h | _MVECTBGRNDACTIVE | Active register for MVECTBGRND. | EALLOW | Go |
C0h | _MPSACTL | CLA PSA Control Register | EALLOW | Go |
C2h | _MPSA1 | CLA PSA1 Register | EALLOW | Go |
C4h | _MPSA2 | CLA PSA2 Register | EALLOW | Go |
E0h | SOFTINTEN | CLA Software Interrupt Enable Register | Go | |
E2h | SOFTINTFRC | CLA Software Interrupt Force Register | Go |
Complex bit access types are encoded to fit into small table cells. Table 8-24 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
R-0 | R -0 | Read Returns 0s |
Write Type | ||
W | W | Write |
W1S | W 1S | Write 1 to set |
Reset or Default Value | ||
-n | Value after reset or the default value | |
Register Array Variables | ||
i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. |
_MVECTBGRNDACTIVE is shown in Figure 8-2 and described in Table 8-25.
Return to the Summary Table.
Gives the current interrupted MPC value of the background task, if the background task was running and interrupted, or reflects the MVECTBGRND value, if MCTLBGRND.BGSTART bit is 0.
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
i16 | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
i16 | |||||||
R-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | i16 | R | 0h | Gives the current interrupted MPC value of the background task, if the background task was running and interrupted, or reflects the MVECTBGRND value, if MCTLBGRND.BGSTART bit is 0. Reset type: SYSRSn |
_MPSACTL is shown in Figure 8-3 and described in Table 8-26.
Return to the Summary Table.
PSA Control Register
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
MPSA2CFG | MPSA2CLEAR | MPSA1CLEAR | MDWDBCYC | MDWDBSTART | MPABCYC | MPABSTART | |
R/W-0h | R-0/W1S-0h | R-0/W1S-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-8 | RESERVED | R | 0h | Reserved |
7-6 | MPSA2CFG | R/W | 0h | CLA PSA2 Polynomial Configuration Bits: These bits configure the type of polynomial used for PSA2. The polynomials chosen are commonly used in the industry: Mode Polynomial Type 0,0 PSA 0,1 CRC32 1,0 CRC16 1,1 CRC16-CCITT Note: [1] Polynomial configuration should be performed when PSA2 is stopped. Reset type: SYSRSn |
5 | MPSA2CLEAR | R-0/W1S | 0h | CLA PSA2 Clear Bit: Writing of '1' will clear contents of PSA2 register. Writes of '0' are ignored. Always reads back a '0' Note: Clearing operation should be performed when PSA2 is stopped. Reset type: SYSRSn |
4 | MPSA1CLEAR | R-0/W1S | 0h | CLA PSA1 Clear Bit: Writing of '1' will clear contents of PSA1 register. Writes of '0' are ignored. Always reads back a '0' Note: Clearing operation should be performed when PSA1 is stopped. Reset type: SYSRSn |
3 | MDWDBCYC | R/W | 0h | CLA Data Write Data Bus PSA2 Cycle or Event Based Bit: 0 PSA2 calculated on every cycle 1 PSA2 calculated on every bus event Reset type: SYSRSn |
2 | MDWDBSTART | R/W | 0h | CLA Data Write Data Bus PSA2 Start/Stop Bit: 0 PSA2 stopped 1 PSA2 start Reset type: SYSRSn |
1 | MPABCYC | R/W | 0h | CLA Program Address Bus PSA1 Cycle/Event Based Bit: 0 PSA1 calculated on every cycle 1 PSA1 calculated on every bus event Reset type: SYSRSn |
0 | MPABSTART | R/W | 0h | CLA Program Address Bus PSA1 Start/Stop Bit: 0 PSA1 stopped 1 PSA1 start Reset type: SYSRSn |
_MPSA1 is shown in Figure 8-4 and described in Table 8-27.
Return to the Summary Table.
PSA1 Register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
i32 | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | i32 | R/W | 0h | PSA1 Value: Reading this register gives the current PSA1 value. The value can be read at any time. Writes to this register are allowed to initialize the PSA1 to a known value. Writes to this register should only be made when PSA1 is stopped. Register value is cleared to zero by reset or by writing to the MPSA1CLEAR bit in the MPSACTL register. Reset type: SYSRSn |
_MPSA2 is shown in Figure 8-5 and described in Table 8-28.
Return to the Summary Table.
PSA2 Register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
i32 | |||||||||||||||||||||||||||||||
R/W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | i32 | R/W | 0h | PSA2 Value: Reading this register gives the current PSA2 value. The value can be read at any time. Writes to this register are allowed to initialize the PSA2 to a known value. Writes to this register should only be made when PSA2 is stopped. Register value is cleared to zero by reset or by writing to the MPSA2CLEAR bit in the MPSACTL register. Reset type: SYSRSn |
SOFTINTEN is shown in Figure 8-6 and described in Table 8-29.
Return to the Summary Table.
Enables the ability to generate CLA task interrupt from within the task, by writing to SOFTINTFRC register. SOFTINTFRC register can only be written from CLA.
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R/W-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
TASK8 | TASK7 | TASK6 | TASK5 | TASK4 | TASK3 | TASK2 | TASK1 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-8 | RESERVED | R/W | 0h | Reserved |
7 | TASK8 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
6 | TASK7 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
5 | TASK6 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
4 | TASK5 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
3 | TASK4 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
2 | TASK3 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
1 | TASK2 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
0 | TASK1 | R/W | 0h | 0: End-Of-Task Interrupt is fired for the respective task 1: Enable Software Interrupt for the respective task. End-of-Task interrupt is not sent to CPU in this case. Note: SOFTINTEN register is read only in the CPU memory map. Reset type: SYSRSn |
SOFTINTFRC is shown in Figure 8-7 and described in Table 8-30.
Return to the Summary Table.
Writing a value of 1 in a bit will generate the corresponding task interrupt.
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R/W-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
TASK8 | TASK7 | TASK6 | TASK5 | TASK4 | TASK3 | TASK2 | TASK1 |
R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-8 | RESERVED | R/W | 0h | Reserved |
7 | TASK8 | R-0/W1S | 0h | Write of '1' will generate a CLA software interrupt to the CPU for the corresponding task. Write of '0' has no effect. Reset type: SYSRSn |
6 | TASK7 | R-0/W1S | 0h | Write of '1' will generate a CLA software interrupt to the CPU for the corresponding task. Write of '0' has no effect. Reset type: SYSRSn |
5 | TASK6 | R-0/W1S | 0h | Write of '1' will generate a CLA software interrupt to the CPU for the corresponding task. Write of '0' has no effect. Reset type: SYSRSn |
4 | TASK5 | R-0/W1S | 0h | Write of '1' will generate a CLA software interrupt to the CPU for the corresponding task. Write of '0' has no effect. Reset type: SYSRSn |
3 | TASK4 | R-0/W1S | 0h | Write of '1' will generate a CLA software interrupt to the CPU for the corresponding task. Write of '0' has no effect. Reset type: SYSRSn |
2 | TASK3 | R-0/W1S | 0h | Write of '1' will generate a CLA software interrupt to the CPU for the corresponding task. Write of '0' has no effect. Reset type: SYSRSn |
1 | TASK2 | R-0/W1S | 0h | Write of '1' will generate a CLA software interrupt to the CPU for the corresponding task. Write of '0' has no effect. Reset type: SYSRSn |
0 | TASK1 | R-0/W1S | 0h | Write of '1' will generate a CLA software interrupt to the CPU for the corresponding task. Write of '0' has no effect. Reset type: SYSRSn |