SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Table 48-2 lists the memory-mapped registers for the UART_REGS registers. All register offset addresses not listed in Table 48-2 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Write Protection | Section |
---|---|---|---|---|
0h | UARTDR | UART Data | Go | |
4h | UARTRSR | UART Receive Status/Error Clear | Go | |
18h | UARTFR | UART Flag | Go | |
20h | UARTILPR | UART IrDA Low-Power Register | Go | |
24h | UARTIBRD | UART Integer Baud-Rate Divisor | Go | |
28h | UARTFBRD | UART Fractional Baud-Rate Divisor | Go | |
2Ch | UARTLCRH | UART Line Control | Go | |
30h | UARTCTL | UART Control | Go | |
34h | UARTIFLS | UART Interrupt FIFO Level Select | Go | |
38h | UARTIM | UART Interrupt Mask | Go | |
3Ch | UARTRIS | UART Raw Interrupt Status | Go | |
40h | UARTMIS | UART Masked Interrupt Status | Go | |
44h | UARTICR | UART Interrupt Clear | Go | |
48h | UARTDMACTL | UART DMA Control | Go | |
A4h | UART9BITADDR | UART 9-Bit Self Address | Go | |
A8h | UART9BITAMASK | UART 9-Bit Self Address Mask | Go | |
FC0h | UARTPP | UART Peripheral Properties | Go | |
FD0h | UARTPeriphID4 | UART Peripheral Identification 4 | Go | |
FD4h | UARTPeriphID5 | UART Peripheral Identification 5 | Go | |
FD8h | UARTPeriphID6 | UART Peripheral Identification 6 | Go | |
FDCh | UARTPeriphID7 | UART Peripheral Identification 7 | Go | |
FE0h | UARTPeriphID0 | UART Peripheral Identification 0 | Go | |
FE4h | UARTPeriphID1 | UART Peripheral Identification 1 | Go | |
FE8h | UARTPeriphID2 | UART Peripheral Identification 2 | Go | |
FECh | UARTPeriphID3 | UART Peripheral Identification 3 | Go | |
FF0h | UARTPCellID0 | UART PrimeCell Identification 0 | Go | |
FF4h | UARTPCellID1 | UART PrimeCell Identification 1 | Go | |
FF8h | UARTPCellID2 | UART PrimeCell Identification 2 | Go | |
FFCh | UARTPCellID3 | UART PrimeCell Identification 3 | Go |
Complex bit access types are encoded to fit into small table cells. Table 48-3 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
R-0 | R -0 | Read Returns 0s |
Write Type | ||
W | W | Write |
W1S | W 1S | Write 1 to set |
Reset or Default Value | ||
-n | Value after reset or the default value | |
Register Array Variables | ||
i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. |
UARTDR is shown in Figure 48-4 and described in Table 48-4.
Return to the Summary Table.
IMPORTANT: This register is read sensitive. This register is the data register (the interface to the FIFOs).
For transmitted data, if the FIFO is enabled, data written to this location is pushed onto the transmit
FIFO. If the FIFO is disabled, data is stored in the transmitter holding register (the bottom word of
the transmit FIFO). A write to this register initiates a transmission from the UART.
For received data, if the FIFO is enabled, the data byte and the 4-bit status (break, frame, parity,
and overrun) is pushed onto the 12-bit wide receive FIFO. If the FIFO is disabled, the data byte and
status are stored in the receiving holding register (the bottom word of the receive FIFO). The received
data can be retrieved by reading this register.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0h | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | OE | BE | PE | FE | DATA | ||||||||||
R-0h | R-0h | R-0h | R-0h | R-0h | R/W-0h | ||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-12 | RESERVED | R | 0h | Reserved |
11 | OE | R | 0h | UART Overrun Error 0 No data has been lost due to a FIFO overrun. 1 New data was received when the FIFO was full, resulting in data loss. Reset type: PER.RESET |
10 | BE | R | 0h | UART Break Error 0 No break condition has occurred 1 A break condition has been detected, indicating that the receive data input was held Low for longer than a full-word transmission time (defined as start, data, parity, and stop bits). In FIFO mode, this error is associated with the character at the top of the FIFO. When a break occurs, only one 0 character is loaded into the FIFO. The next character is only enabled after the received data input goes to a 1 (marking state), and the next valid start bit is received. Reset type: PER.RESET |
9 | PE | R | 0h | UART Parity Error 0 No parity error has occurred 1 The parity of the received data character does not match the parity defined by bits 2 and 7 of the UARTLCRH register. In FIFO mode, this error is associated with the character at the top of the FIFO. Reset type: PER.RESET |
8 | FE | R | 0h | UART Framing Error 0 No framing error has occurred 1 The received character does not have a valid stop bit (a valid stop bit is 1). Reset type: PER.RESET |
7-0 | DATA | R/W | 0h | Data Transmitted or Received Data that is to be transmitted via the UART is written to this field. When read, this field contains the data that was received by the UART. For transmitted data, if the FIFO is enabled, data written to this location is pushed onto the transmit FIFO. If the FIFO is disabled, data is stored in the transmitter holding register (the bottom word of the transmit FIFO). A write to this register initiates a transmission from the UART. For received data, if the FIFO is enabled, the data byte and the 4-bit status (break, frame, parity, and overrun) is pushed onto the 12-bit wide receive FIFO. If the FIFO is disabled, the data byte and status are stored in the receiving holding register (the bottom word of the receive FIFO). The received data can be retrieved by reading this register. Reset type: PER.RESET |
UARTRSR is shown in Figure 48-5 and described in Table 48-5.
Return to the Summary Table.
The UARTRSR/UARTECR register is the receive status register/error clear register.
In addition to the UARTDR register, receive status can also be read from the UARTRSR register.
If the status is read from this register, then the status information corresponds to the entry read from
UARTDR prior to reading UARTRSR. The status information for overrun is set immediately when
an overrun condition occurs.
The UARTRSR register cannot be written.
A write of any value to the UARTECR register clears the framing, parity, break, and overrun errors.
All the bits are cleared on reset.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0h | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | OE | BE | PE | FE | |||||||||||
R-0h | R-0h | R-0h | R-0h | R-0h | |||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-4 | RESERVED | R | 0h | Reserved |
3 | OE | R | 0h | UART Overrun Error 0 No data has been lost due to a FIFO overrun. 1 New data was received when the FIFO was full, resulting in data loss. This bit is cleared by a write to UARTECR.The FIFO contents remain valid because no further data is written when the FIFO is full, only the contents of the shift register are overwritten. The CPU must read the data in order to empty the FIFO. Reset type: PER.RESET |
2 | BE | R | 0h | UART Break Error 0 No break condition has occurred 1 A break condition has been detected, indicating that the receive data input was held Low for longer than a full-word transmission time (defined as start, data, parity, and stop bits). This bit is cleared to 0 by a write to UARTECR. In FIFO mode, this error is associated with the character at the top of the FIFO. When a break occurs, only one 0 character is loaded into the FIFO. The next character is only enabled after the receive data input goes to a 1 (marking state) and the next valid start bit is received. Reset type: PER.RESET |
1 | PE | R | 0h | UART Parity Error 0 No parity error has occurred 1 The parity of the received data character does not match the parity defined by bits 2 and 7 of the UARTLCRH register. This bit is cleared to 0 by a write to UARTECR. Reset type: PER.RESET |
0 | FE | R | 0h | UART Framing Error 0 No framing error has occurred 1 The received character does not have a valid stop bit (a valid stop bit is 1). This bit is cleared to 0 by a write to UARTECR. In FIFO mode, this error is associated with the character at the top of the FIFO. Reset type: PER.RESET |
UARTFR is shown in Figure 48-6 and described in Table 48-6.
Return to the Summary Table.
The UARTFR register is the flag register. After reset, the TXFF, RXFF, and BUSY bits are 0, and
TXFE and RXFE bits are 1.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | RESERVED | ||||||
R-0h | R-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
TXFE | RXFF | TXFF | RXFE | BUSY | RESERVED | RESERVED | RESERVED |
R-1h | R-0h | R-0h | R-1h | R-0h | R-0h | R-0h | R-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-9 | RESERVED | R | 0h | Reserved |
8 | RESERVED | R | 0h | Reserved |
7 | TXFE | R | 1h | UART Transmit FIFO Empty The meaning of this bit depends on the state of the FEN bit in the UARTLCRH register. 0 The transmitter has data to transmit. 1 If the FIFO is disabled (FEN is 0), the transmit holding register is empty. If the FIFO is enabled (FEN is 1), the transmit FIFO is empty. Reset type: PER.RESET |
6 | RXFF | R | 0h | UART Receive FIFO Full The meaning of this bit depends on the state of the FEN bit in the UARTLCRH register. 0 The receiver can receive data. 1 If the FIFO is disabled (FEN is 0), the receive holding register is full. If the FIFO is enabled (FEN is 1), the receive FIFO is full. Reset type: PER.RESET |
5 | TXFF | R | 0h | UART Transmit FIFO Full The meaning of this bit depends on the state of the FEN bit in the UARTLCRH register. 0 The transmitter is not full. 1 If the FIFO is disabled (FEN is 0), the transmit holding register is full. If the FIFO is enabled (FEN is 1), the transmit FIFO is full. Reset type: PER.RESET |
4 | RXFE | R | 1h | UART Receive FIFO Empty The meaning of this bit depends on the state of the FEN bit in the UARTLCRH register. 0 The receiver is not empty. 1 If the FIFO is disabled (FEN is 0), the receive holding register is empty. If the FIFO is enabled (FEN is 1), the receive FIFO is empty. Reset type: PER.RESET |
3 | BUSY | R | 0h | UART Busy 0 The UART is not busy. 1 The UART is busy transmitting data. This bit remains set until the complete byte, including all stop bits, has been sent from the shift register. This bit is set as soon as the transmit FIFO becomes non-empty (regardless of whether UART is enabled). Reset type: PER.RESET |
2 | RESERVED | R | 0h | Reserved |
1 | RESERVED | R | 0h | Reserved |
0 | RESERVED | R | 0h | Reserved |
UARTILPR is shown in Figure 48-7 and described in Table 48-7.
Return to the Summary Table.
The UARTILPR register stores the 8-bit low-power counter divisor value used to derive the low-power
SIR pulse width clock.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | ILPDVSR | ||||||||||||||||||||||||||||||
R-0h | R/W-0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | ILPDVSR | R/W | 0h | IrDA Low-Power Divisor This field contains the 8-bit low-power divisor value. The UARTILPR register stores the 8-bit low-power counter divisor value used to derive the low-power SIR pulse width clock by dividing down the system clock (SysClk). All the bits are cleared when reset. The internal IrLPBaud16 clock is generated by dividing down SysClk according to the low-power divisor value written to UARTILPR. The duration of SIR pulses generated when low-power mode is enabled is three times the period of the IrLPBaud16 clock. The low-power divisor value is calculated as follows: ILPDVSR = SysClk / FIrLPBaud16 where FIrLPBaud16 is nominally 1.8432 MHz. Because the IrLPBaud16 clock is used to sample transmitted data irrespective of mode, the ILPDVSR field must be programmed in both low power and normal mode,such that FIrLPBaud16 is between 1.42 and 2.12 MHz, resulting in a low-power pulse duration of 1.41-2.11 us (three times the period of IrLPBaud16). The minimum frequency of IrLPBaud16 ensures that pulses less than one period of IrLPBaud16 are rejected, but pulses greater than 1.4 us are accepted as valid pulses. Note: Zero is an illegal value. Programming a zero value results in no IrLPBaud16 pulses being generated Reset type: PER.RESET |
UARTIBRD is shown in Figure 48-8 and described in Table 48-8.
Return to the Summary Table.
The UARTIBRD register is the integer part of the baud-rate divisor value. All the bits are cleared
on reset. The minimum possible divide ratio is 1 (when UARTIBRD=0), in which case the UARTFBRD
register is ignored. When changing the UARTIBRD register, the new value does not take effect until
transmission/reception of the current character is complete. Any changes to the baud-rate divisor
must be followed by a write to the UARTLCRH register.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIVINT | ||||||||||||||||||||||||||||||
R-0h | R/W-0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15-0 | DIVINT | R/W | 0h | Integer Baud-Rate Divisor The minimum possible divide ratio is 1 (when UARTIBRD=0), in which case the UARTFBRD register is ignored. When changing the UARTIBRD register, the new value does not take effect until transmission/reception of the current character is complete. Any changes to the baud-rate divisor must be followed by a write to the UARTLCRH register. Reset type: PER.RESET |
UARTFBRD is shown in Figure 48-9 and described in Table 48-9.
Return to the Summary Table.
The UARTFBRD register is the fractional part of the baud-rate divisor value. All the bits are cleared
on reset. When changing the UARTFBRD register, the new value does not take effect until
transmission/reception of the current character is complete. Any changes to the baud-rate divisor
must be followed by a write to the UARTLCRH register. See 'Baud-Rate Generation' on page 1165
for configuration details.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0h | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIVFRAC | ||||||||||||||
R-0h | R/W-0h | ||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-6 | RESERVED | R | 0h | Reserved |
5-0 | DIVFRAC | R/W | 0h | Fractional Baud-Rate Divisor The UARTFBRD register is the fractional part of the baud-rate divisor value. All the bits are cleared on reset. When changing the UARTFBRD register, the new value does not take effect until transmission/reception of the current character is complete. Any changes to the baud-rate divisor must be followed by a write to the UARTLCRH register. Reset type: PER.RESET |
UARTLCRH is shown in Figure 48-10 and described in Table 48-10.
Return to the Summary Table.
The UARTLCRH register is the line control register. Serial parameters such as data length, parity,
and stop bit selection are implemented in this register.
When updating the baud-rate divisor (UARTIBRD and/or UARTIFRD), the UARTLCRH register
must also be written. The write strobe for the baud-rate divisor registers is tied to the UARTLCRH
register.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
SPS | WLEN | FEN | STP2 | EPS | PEN | BRK | |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7 | SPS | R/W | 0h | UART Stick Parity Select UART Stick Parity Select 0 Stick parity is disabled (default) 1 Stick parity is enabled. When bits 1, 2, and 7 of UARTLCRH are set, the parity bit is transmitted and checked as a 0. When bits 1 and 7 are set and 2 is cleared, the parity bit is transmitted and checked as a 1. Reset type: PER.RESET |
6-5 | WLEN | R/W | 0h | UART Word Length The bits indicate the number of data bits transmitted or received in a frame as follows: 0x0 5 bits (default) 0x1 6 bits 0x2 7 bits 0x3 8 bits Reset type: PER.RESET |
4 | FEN | R/W | 0h | UART Enable FIFOs 0 The FIFOs are disabled. The FIFOs become 1-byte-deep holding registers. 1 The transmit and receive FIFO buffers are enabled (FIFO mode). Reset type: PER.RESET |
3 | STP2 | R/W | 0h | UART Two Stop Bits Select 0 One stop bit is transmitted at the end of a frame. 1 Two stop bits are transmitted at the end of a frame. The receive logic does not check for two stop bits being received. Reset type: PER.RESET |
2 | EPS | R/W | 0h | UART Even Parity Select 0 Odd parity is performed, which checks for an odd number of 1s. 1 Even parity generation and checking is performed during transmission and reception, which checks for an even number of 1s in data and parity bits. This bit has no effect when parity is disabled by the PEN bit. Reset type: PER.RESET |
1 | PEN | R/W | 0h | UART Parity Enable 0 Parity is disabled and no parity bit is added to the data frame. 1 Parity checking and generation is enabled. Reset type: PER.RESET |
0 | BRK | R/W | 0h | UART Send Break 0 Normal use. 1 A Low level is continually output on the UnTx signal, after completing transmission of the current character. For the proper execution of the break command, software must set this bit for at least two frames (character periods). Reset type: PER.RESET |
UARTCTL is shown in Figure 48-11 and described in Table 48-11.
Return to the Summary Table.
The UARTCTL register is the control register. All the bits are cleared on reset except for the Transmit
Enable (TXE) and Receive Enable (RXE) bits, which are set.
To enable the UART module, the UARTEN bit must be set. If software requires a configuration change
in the module, the UARTEN bit must be cleared before the configuration changes are written. If the
UART is disabled during a transmit or receive operation, the current transaction is completed prior
to the UART stopping.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | RXE | TXE | |
R/W-0h | R/W-0h | R-0h | R/W-0h | R/W-0h | R/W-1h | R/W-1h | |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
LBE | RESERVED | HSE | EOT | RESERVED | SIRLP | SIREN | UARTEN |
R/W-0h | R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15 | RESERVED | R/W | 0h | Reserved |
14 | RESERVED | R/W | 0h | Reserved |
13-12 | RESERVED | R | 0h | Reserved |
11 | RESERVED | R/W | 0h | Reserved |
10 | RESERVED | R/W | 0h | Reserved |
9 | RXE | R/W | 1h | UART Receive Enable 0 The receive section of the UART is disabled. 1 The receive section of the UART is enabled. If the UART is disabled in the middle of a receive, it completes the current character before stopping.To enable reception, the UARTEN bit must also be set. Reset type: PER.RESET |
8 | TXE | R/W | 1h | UART Transmit Enable 0 The transmit section of the UART is disabled. 1 The transmit section of the UART is enabled. If the UART is disabled in the middle of a transmission, it completes the current character before stopping. To enable transmission, the UARTEN bit must also be set. Reset type: PER.RESET |
7 | LBE | R/W | 0h | UART Loop Back Enable 0 Normal operation. 1 The UnTx path is fed through the UnRx path. Reset type: PER.RESET |
6 | RESERVED | R | 0h | Reserved |
5 | HSE | R/W | 0h | High-Speed Enable 0 The UART is clocked using the system clock divided by 16. 1 The UART is clocked using the system clock divided by 8. Reset type: PER.RESET |
4 | EOT | R/W | 0h | End of Transmission This bit determines the behavior of the TXRIS bit in the UARTRIS register. 0 The TXRIS bit is set when the transmit FIFO condition specified in UARTIFLS is met. 1 The TXRIS bit is set only after all transmitted data, including stop bits, have cleared the serializer. Reset type: PER.RESET |
3 | RESERVED | R/W | 0h | Reserved |
2 | SIRLP | R/W | 0h | UART SIR Low-Power Mode This bit selects the IrDA encoding mode. 0 Low-level bits are transmitted as an active High pulse with a width of 3/16th of the bit period. 1 The UART operates in SIR Low-Power mode. Low-level bits are transmitted with a pulse width which is 3 times the period of the IrLPBaud16 input signal, regardless of the selected bit rate. Setting this bit uses less power, but might reduce transmission distances. Reset type: PER.RESET |
1 | SIREN | R/W | 0h | UART SIR Enable 0 Normal operation. 1 The IrDA SIR block is enabled, and the UART will transmit and receive data using SIR protocol. Reset type: PER.RESET |
0 | UARTEN | R/W | 0h | UART Enable 0 The UART is disabled. 1 The UART is enabled. If the UART is disabled in the middle of transmission or reception, it completes the current character before stopping. Reset type: PER.RESET |
UARTIFLS is shown in Figure 48-12 and described in Table 48-12.
Return to the Summary Table.
The UARTIFLS register is the interrupt FIFO level select register. You can use this register to define the FIFO level at which the TXRIS and RXRIS bits in the UARTRIS register are triggered.
The interrupts are generated based on a transition through a level rather than being based on the level. That is, the interrupts are generated when the fill level progresses through the trigger level.
For example, if the receive trigger level is set to the half-way mark, the interrupt is triggered as the module is receiving the 9th character.
Therefore, changing the trigger level does not trigger an interrupt using the new level until another character is received.
Out of reset, the TXIFLSEL and RXIFLSEL bits are configured so that the FIFOs trigger an interrupt at the half-way mark.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0h | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | RXIFLSEL | TXIFLSEL | |||||||||||||
R-0h | R/W-2h | R/W-2h | |||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-6 | RESERVED | R | 0h | Reserved |
5-3 | RXIFLSEL | R/W | 2h | UART Receive Interrupt FIFO Level Select The trigger points for the receive interrupt are as follows: Value Description 0x0 RX FIFO greater than or equal to 1/8 full - at least 2 filled spots 0x1 RX FIFO greater than or equal to 1/4 full - at least 4 filled spots 0x2 RX FIFO greater than or equal to 1/2 full - at least 8 filled spots (default) 0x3 RX FIFO greater than or equal to 3/4 full - at least 12 filled spots 0x4 RX FIFO greater than or equal to 7/8 full - at least 14 filled spots 0x5-0x7 Reserved Reset type: PER.RESET |
2-0 | TXIFLSEL | R/W | 2h | Value Description 0x0 TX FIFO less than or equal to 1/8 full - at least 14 empty spots 0x1 TX FIFO less than or equal to 1/4 full - at least 12 empty spots 0x2 TX FIFO less than or equal to 1/2 full - at least 8 empty spots (default) 0x3 TX FIFO less than or equal to 3/4 full - at least 4 empty spots 0x4 TX FIFO less than or equal to 7/8 full - at least 2 empty spots 0x5-0x7 Reserved Note: If the EOT bit in UARTCTL is set, the transmit interrupt is generated once the FIFO is completely empty and all data including stop bits have left the transmit serializer. In this case, the setting of TXIFLSEL is ignored. Reset type: PER.RESET |
UARTIM is shown in Figure 48-13 and described in Table 48-13.
Return to the Summary Table.
The UARTIM register is the interrupt mask set/clear register.
On a read, this register gives the current value of the mask on the relevant interrupt. Setting a bit
allows the corresponding raw interrupt signal to be routed to the interrupt controller. Clearing a bit
prevents the raw interrupt signal from being sent to the interrupt controller.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DMATXIM | DMARXIM | |||||
R-0h | R/W-0h | R/W-0h | |||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | 9BITIM | RESERVED | OEIM | BEIM | PEIM | ||
R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
FEIM | RTIM | TXIM | RXIM | RESERVED | RESERVED | RESERVED | RESERVED |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-18 | RESERVED | R | 0h | Reserved |
17 | DMATXIM | R/W | 0h | Transmit DMA Interrupt Mask 0 The DMATXRIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the DMATXRIS bit in the UARTRIS register is set. Reset type: PER.RESET |
16 | DMARXIM | R/W | 0h | Receive DMA Interrupt Mask 0 The DMARXRIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the DMARXRIS bit in the UARTRIS register is set. Reset type: PER.RESET |
15-13 | RESERVED | R | 0h | Reserved |
12 | 9BITIM | R/W | 0h | 9-Bit Mode Interrupt Mask 0 The 9BITRIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the 9BITRIS bit in the UARTRIS register is set. Reset type: PER.RESET |
11 | RESERVED | R/W | 0h | Reserved |
10 | OEIM | R/W | 0h | UART Overrun Error Interrupt Mask 0 The OERIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the OERIS bit in the UARTRIS register is set. Reset type: PER.RESET |
9 | BEIM | R/W | 0h | UART Break Error Interrupt Mask 0 The BERIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the BERIS bit in the UARTRIS register is set. Reset type: PER.RESET |
8 | PEIM | R/W | 0h | UART Parity Error Interrupt Mask 0 The PERIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the PERIS bit in the UARTRIS register is set. Reset type: PER.RESET |
7 | FEIM | R/W | 0h | UART Framing Error Interrupt Mask 0 The FERIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the FERIS bit in the UARTRIS register is set. Reset type: PER.RESET |
6 | RTIM | R/W | 0h | UART Receive Time-Out Interrupt Mask 0 The RTRIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the RTRIS bit in the UARTRIS register is set. Reset type: PER.RESET |
5 | TXIM | R/W | 0h | UART Transmit Interrupt Mask 0 The TXRIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the TXRIS bit in the UARTRIS register is set. Reset type: PER.RESET |
4 | RXIM | R/W | 0h | UART Receive Interrupt Mask 0 The RXRIS interrupt is suppressed and not sent to the interrupt controller. 1 An interrupt is sent to the interrupt controller when the RXRIS bit in the UARTRIS register is set. Reset type: PER.RESET |
3 | RESERVED | R/W | 0h | Reserved |
2 | RESERVED | R/W | 0h | Reserved |
1 | RESERVED | R/W | 0h | Reserved |
0 | RESERVED | R/W | 0h | Reserved |
UARTRIS is shown in Figure 48-14 and described in Table 48-14.
Return to the Summary Table.
The UARTRIS register is the raw interrupt status register. On a read, this register gives the current
raw status value of the corresponding interrupt. A write has no effect.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DMATXRIS | DMARXRIS | |||||
R-0h | R-0h | R-0h | |||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | 9BITRIS | RESERVED | OERIS | BERIS | PERIS | ||
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | ||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
FERIS | RTRIS | TXRIS | RXRIS | RESERVED | RESERVED | RESERVED | RESERVED |
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-18 | RESERVED | R | 0h | Reserved |
17 | DMATXRIS | R | 0h | Transmit DMA Raw Interrupt Status 0 No interrupt 1 The transmit DMA has completed. This bit is cleared by writing a 1 to the DMATXIC bit in the UARTICR register. Reset type: PER.RESET |
16 | DMARXRIS | R | 0h | Receive DMA Raw Interrupt Status 0 No interrupt 1 The receive DMA has completed. This bit is cleared by writing a 1 to the DMARXIC bit in the UARTICR register. Reset type: PER.RESET |
15-13 | RESERVED | R | 0h | Reserved |
12 | 9BITRIS | R | 0h | 9-Bit Mode Raw Interrupt Status 0 No interrupt 1 A receive address match has occurred. This bit is cleared by writing a 1 to the 9BITIC bit in the UARTICR register. Reset type: PER.RESET |
11 | RESERVED | R | 0h | Reserved |
10 | OERIS | R | 0h | UART Overrun Error Raw Interrupt Status 0 No interrupt 1 An overrun error has occurred. This bit is cleared by writing a 1 to the OEIC bit in the UARTICR register. Reset type: PER.RESET |
9 | BERIS | R | 0h | UART Break Error Raw Interrupt Status 0 No interrupt 1 A break error has occurred. This bit is cleared by writing a 1 to the BEIC bit in the UARTICR register. Reset type: PER.RESET |
8 | PERIS | R | 0h | UART Parity Error Raw Interrupt Status 0 No interrupt 1 A parity error has occurred. This bit is cleared by writing a 1 to the PEIC bit in the UARTICR register. Reset type: PER.RESET |
7 | FERIS | R | 0h | UART Framing Error Raw Interrupt Status 0 No interrupt 1 A framing error has occurred. This bit is cleared by writing a 1 to the FEIC bit in the UARTICR register. Reset type: PER.RESET |
6 | RTRIS | R | 0h | UART Receive Time-Out Raw Interrupt Status 0 No interrupt 1 A receive time out has occurred. This bit is cleared by writing a 1 to the RTIC bit in the UARTICR register. Reset type: PER.RESET |
5 | TXRIS | R | 0h | UART Transmit Raw Interrupt Status 0 No interrupt 1 If the EOT bit in the UARTCTL register is clear, the transmit FIFO level has passed through the condition defined in the UARTIFLS register.If the EOT bit is set, the last bit of all transmitted data and flags has left the serializer. This bit is cleared by writing a 1 to the TXIC bit in the UARTICR register or by writing data to the transmit FIFO until it becomes greater than the trigger level, if the FIFO is enabled, or by writing a single byte if the FIFO is disabled. Reset type: PER.RESET |
4 | RXRIS | R | 0h | UART Receive Raw Interrupt Status 0 No interrupt 1 The receive FIFO level has passed through the condition defined in the UARTIFLS register. This bit is cleared by writing a 1 to the RXIC bit in the UARTICR register or by reading data from the receive FIFO until it becomes less than the trigger level, if the FIFO is enabled, or by reading a single byte if the FIFO is disabled. Reset type: PER.RESET |
3 | RESERVED | R | 0h | Reserved |
2 | RESERVED | R | 0h | Reserved |
1 | RESERVED | R | 0h | Reserved |
0 | RESERVED | R | 0h | Reserved |
UARTMIS is shown in Figure 48-15 and described in Table 48-15.
Return to the Summary Table.
The UARTMIS register is the masked interrupt status register. On a read, this register gives the
current masked status value of the corresponding interrupt. A write has no effect.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DMATXMIS | DMARXMIS | |||||
R-0h | R-0h | R-0h | |||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | 9BITMIS | RESERVED | OEMIS | BEMIS | PEMIS | ||
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | ||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
FEMIS | RTMIS | TXMIS | RXMIS | RESERVED | RESERVED | RESERVED | RESERVED |
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-18 | RESERVED | R | 0h | Reserved |
17 | DMATXMIS | R | 0h | Transmit DMA Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to the completion of the transmit DMA. This bit is cleared by writing a 1 to the DMATXIC bit in the UARTICR register. Reset type: PER.RESET |
16 | DMARXMIS | R | 0h | Receive DMA Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to the completion of the receive DMA. This bit is cleared by writing a 1 to the DMARXIC bit in the UARTICR register. Reset type: PER.RESET |
15-13 | RESERVED | R | 0h | Reserved |
12 | 9BITMIS | R | 0h | 9-Bit Mode Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to a receive address match. This bit is cleared by writing a 1 to the 9BITIC bit in the UARTICR register. Reset type: PER.RESET |
11 | RESERVED | R | 0h | Reserved |
10 | OEMIS | R | 0h | UART Overrun Error Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to an overrun error. This bit is cleared by writing a 1 to the OEIC bit in the UARTICR register. Reset type: PER.RESET |
9 | BEMIS | R | 0h | UART Break Error Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to a break error. This bit is cleared by writing a 1 to the BEIC bit in the UARTICR register. Reset type: PER.RESET |
8 | PEMIS | R | 0h | UART Parity Error Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to a parity error. This bit is cleared by writing a 1 to the PEIC bit in the UARTICR register. Reset type: PER.RESET |
7 | FEMIS | R | 0h | UART Framing Error Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to a framing error. This bit is cleared by writing a 1 to the FEIC bit in the UARTICR register. Reset type: PER.RESET |
6 | RTMIS | R | 0h | UART Receive Time-Out Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to a receive time out. This bit is cleared by writing a 1 to the RTIC bit in the UARTICR register. Reset type: PER.RESET |
5 | TXMIS | R | 0h | UART Transmit Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to passing through the specified transmit FIFO level (if the EOT bit is clear) or due to the transmission of the last data bit (if the EOT bit is set). This bit is cleared by writing a 1 to the TXIC bit in the UARTICR register or by writing data to the transmit FIFO until it becomes greater than the trigger level, if the FIFO is enabled, or by writing a single byte if the FIFO is disabled. Reset type: PER.RESET |
4 | RXMIS | R | 0h | UART Receive Masked Interrupt Status 0 An interrupt has not occurred or is masked. 1 An unmasked interrupt was signaled due to passing through the specified receive FIFO level. This bit is cleared by writing a 1 to the RXIC bit in the UARTICR register or by reading data from the receive FIFO until it becomes less than the trigger level, if the FIFO is enabled, or by reading a single byte if the FIFO is disabled. Reset type: PER.RESET |
3 | RESERVED | R | 0h | Reserved |
2 | RESERVED | R | 0h | Reserved |
1 | RESERVED | R | 0h | Reserved |
0 | RESERVED | R | 0h | Reserved |
UARTICR is shown in Figure 48-16 and described in Table 48-16.
Return to the Summary Table.
The UARTICR register is the interrupt clear register. On a write of 1, the corresponding interrupt
(both raw interrupt and masked interrupt, if enabled) is cleared. A write of 0 has no effect.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DMATXIC | DMARXIC | |||||
R-0h | R-0/W1S-0h | R-0/W1S-0h | |||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | 9BITIC | EOTIC | OEIC | BEIC | PEIC | ||
R-0h | R/W-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | ||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
FEIC | RTIC | TXIC | RXIC | RESERVED | RESERVED | RESERVED | RESERVED |
R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-18 | RESERVED | R | 0h | Reserved |
17 | DMATXIC | R-0/W1S | 0h | Transmit DMA Interrupt Clear Writing a 1 to this bit clears the DMATXRIS bit in the UARTRIS register and the DMATXMIS bit in the UARTMIS register. Reset type: PER.RESET |
16 | DMARXIC | R-0/W1S | 0h | Receive DMA Interrupt Clear Writing a 1 to this bit clears the DMARXRIS bit in the UARTRIS register and the DMARXMIS bit in the UARTMIS register. Reset type: PER.RESET |
15-13 | RESERVED | R | 0h | Reserved |
12 | 9BITIC | R/W | 0h | 9-Bit Mode Interrupt Clear Writing a 1 to this bit clears the 9BITRIS bit in the UARTRIS register and the 9BITMIS bit in the UARTMIS register. Reset type: PER.RESET |
11 | EOTIC | R-0/W1S | 0h | End of Transmission Interrupt Clear Writing a 1 to this bit clears the EOTRIS bit in the UARTRIS register and the EOTMIS bit in the UARTMIS register. Reset type: PER.RESET |
10 | OEIC | R-0/W1S | 0h | Overrun Error Interrupt Clear Writing a 1 to this bit clears the OERIS bit in the UARTRIS register and the OEMIS bit in the UARTMIS register. Reset type: PER.RESET |
9 | BEIC | R-0/W1S | 0h | Break Error Interrupt Clear Writing a 1 to this bit clears the BERIS bit in the UARTRIS register and the BEMIS bit in the UARTMIS register. Reset type: PER.RESET |
8 | PEIC | R-0/W1S | 0h | Parity Error Interrupt Clear Writing a 1 to this bit clears the PERIS bit in the UARTRIS register and the PEMIS bit in the UARTMIS register. Reset type: PER.RESET |
7 | FEIC | R-0/W1S | 0h | Framing Error Interrupt Clear Writing a 1 to this bit clears the FERIS bit in the UARTRIS register and the FEMIS bit in the UARTMIS register. Reset type: PER.RESET |
6 | RTIC | R-0/W1S | 0h | Receive Time-Out Interrupt Clear Writing a 1 to this bit clears the RTRIS bit in the UARTRIS register and the RTMIS bit in the UARTMIS register. Reset type: PER.RESET |
5 | TXIC | R-0/W1S | 0h | Transmit Interrupt Clear Writing a 1 to this bit clears the TXRIS bit in the UARTRIS register and the TXMIS bit in the UARTMIS register. Reset type: PER.RESET |
4 | RXIC | R-0/W1S | 0h | Receive Interrupt Clear Writing a 1 to this bit clears the RXRIS bit in the UARTRIS register and the RXMIS bit in the UARTMIS register. Reset type: PER.RESET |
3 | RESERVED | R-0/W1S | 0h | Reserved |
2 | RESERVED | R-0/W1S | 0h | Reserved |
1 | RESERVED | R-0/W1S | 0h | Reserved |
0 | RESERVED | R-0/W1S | 0h | Reserved |
UARTDMACTL is shown in Figure 48-17 and described in Table 48-17.
Return to the Summary Table.
UART DMA Control
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DMAERR | TXDMAE | RXDMAE | ||||
R-0h | R/W-0h | R/W-0h | R/W-0h | ||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-3 | RESERVED | R | 0h | Reserved |
2 | DMAERR | R/W | 0h | DMA on Error 0 DMA receive requests are unaffected when a receive error occurs. 1 DMA receive requests are automatically disabled when a receive error occurs. Reset type: PER.RESET |
1 | TXDMAE | R/W | 0h | Transmit DMA Enable 0 DMA for the transmit FIFO is disabled. 1 DMA for the transmit FIFO is enabled. Reset type: PER.RESET |
0 | RXDMAE | R/W | 0h | Receive DMA Enable 0 DMA for the receive FIFO is disabled. 1 DMA for the receive FIFO is enabled. Reset type: PER.RESET |
UART9BITADDR is shown in Figure 48-18 and described in Table 48-18.
Return to the Summary Table.
The UART9BITADDR register is used to write the specific address that should be matched with the
receiving byte when the 9-bit Address Mask (UART9BITAMASK) is set to 0xFF. This register is
used in conjunction with UART9BITAMASK to form a match for address-byte received.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
9BITEN | RESERVED | ||||||
R/W-0h | R-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
ADDR | |||||||
R/W-0h | |||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-16 | RESERVED | R | 0h | Reserved |
15 | 9BITEN | R/W | 0h | Enable 9-Bit Mode 0 9-bit mode is disabled. 1 9-bit mode is enabled. Reset type: PER.RESET |
14-8 | RESERVED | R | 0h | Reserved |
7-0 | ADDR | R/W | 0h | Self Address for 9-Bit Mode This field contains the address that should be matched when UART9BITAMASK is 0xFF. Reset type: PER.RESET |
UART9BITAMASK is shown in Figure 48-19 and described in Table 48-19.
Return to the Summary Table.
The UART9BITAMASK register is used to enable the address mask for 9-bit mode. The address
bits are masked to create a set of addresses to be matched with the received address byte.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | MASK | ||||||||||||||||||||||||||||||
R-0h | R/W-FFh | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | MASK | R/W | FFh | Self Address Mask for 9-Bit Mode This field contains the address mask that creates a set of addresses that should be matched. Reset type: PER.RESET |
UARTPP is shown in Figure 48-20 and described in Table 48-20.
Return to the Summary Table.
The UARTPP register provides information regarding the properties of the UART module.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||||||||||
R-0h | |||||||||||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | MSE | MS | NB | SC | |||||||||||
R-0h | R-0h | R-0h | R-1h | R-0h | |||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-4 | RESERVED | R | 0h | Reserved |
3 | MSE | R | 0h | Modem Support Extended 0 The UART module does not provide extended support for modem control. 1 The UART module provides extended support for modem control including UARTnDTR, UARTnDSR, UARTnDCD, and UARTnRI. Reset type: PER.RESET |
2 | MS | R | 0h | Modem Support 0 The UART module does not provide support for modem control. 1 The UART module provides support for modem control including UARTnRTS and UARTnCTS. Reset type: PER.RESET |
1 | NB | R | 1h | 9-Bit Support 0 The UART module does not provide support for the transmission of 9-bit data for RS-485 support. 1 The UART module provides support for the transmission of 9-bit data for RS-485 support. Reset type: PER.RESET |
0 | SC | R | 0h | Smart Card Support 0 The UART module does not provide smart card support. 1 The UART module provides smart card support. Reset type: PER.RESET |
UARTPeriphID4 is shown in Figure 48-21 and described in Table 48-21.
Return to the Summary Table.
UART Peripheral Identification 4
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PID4 | ||||||||||||||||||||||||||||||
R-0h | R-60h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | PID4 | R | 60h | UART Peripheral ID Register [7:0] Can be used by software to identify the presence of this peripheral. Reset type: PER.RESET |
UARTPeriphID5 is shown in Figure 48-22 and described in Table 48-22.
Return to the Summary Table.
UART Peripheral Identification 5
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PID5 | ||||||||||||||||||||||||||||||
R-0h | R-0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | PID5 | R | 0h | UART Peripheral ID Register [15:8] Can be used by software to identify the presence of this peripheral. Reset type: PER.RESET |
UARTPeriphID6 is shown in Figure 48-23 and described in Table 48-23.
Return to the Summary Table.
UART Peripheral Identification 6
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PID6 | ||||||||||||||||||||||||||||||
R-0h | R-0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | PID6 | R | 0h | UART Peripheral ID Register [23:16] Can be used by software to identify the presence of this peripheral. Reset type: PER.RESET |
UARTPeriphID7 is shown in Figure 48-24 and described in Table 48-24.
Return to the Summary Table.
UART Peripheral Identification 7
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PID7 | ||||||||||||||||||||||||||||||
R-0h | R-0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | PID7 | R | 0h | UART Peripheral ID Register [31:24] Can be used by software to identify the presence of this peripheral. Reset type: PER.RESET |
UARTPeriphID0 is shown in Figure 48-25 and described in Table 48-25.
Return to the Summary Table.
UART Peripheral Identification 0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PID0 | ||||||||||||||||||||||||||||||
R-0h | R-11h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | PID0 | R | 11h | UART Peripheral ID Register [7:0] Can be used by software to identify the presence of this peripheral. Reset type: PER.RESET |
UARTPeriphID1 is shown in Figure 48-26 and described in Table 48-26.
Return to the Summary Table.
UART Peripheral Identification 1
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PID1 | ||||||||||||||||||||||||||||||
R-0h | R-0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | PID1 | R | 0h | UART Peripheral ID Register [15:8] Can be used by software to identify the presence of this peripheral. Reset type: PER.RESET |
UARTPeriphID2 is shown in Figure 48-27 and described in Table 48-27.
Return to the Summary Table.
UART Peripheral Identification 2
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PID2 | ||||||||||||||||||||||||||||||
R-0h | R-18h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | PID2 | R | 18h | UART Peripheral ID Register [23:16] Can be used by software to identify the presence of this peripheral. Reset type: PER.RESET |
UARTPeriphID3 is shown in Figure 48-28 and described in Table 48-28.
Return to the Summary Table.
UART Peripheral Identification 3
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PID3 | ||||||||||||||||||||||||||||||
R-0h | R-1h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | PID3 | R | 1h | UART Peripheral ID Register [31:24] Can be used by software to identify the presence of this peripheral. Reset type: PER.RESET |
UARTPCellID0 is shown in Figure 48-29 and described in Table 48-29.
Return to the Summary Table.
UART PrimeCell Identification 0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | CID0 | ||||||||||||||||||||||||||||||
R-0h | R-Dh | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CID0 | R | Dh | UART PrimeCell ID Register [7:0] Provides software a standard cross-peripheral identification system. Reset type: PER.RESET |
UARTPCellID1 is shown in Figure 48-30 and described in Table 48-30.
Return to the Summary Table.
UART PrimeCell Identification 1
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | CID1 | ||||||||||||||||||||||||||||||
R-0h | R-F0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CID1 | R | F0h | UART PrimeCell ID Register [15:8] Provides software a standard cross-peripheral identification system. Reset type: PER.RESET |
UARTPCellID2 is shown in Figure 48-31 and described in Table 48-31.
Return to the Summary Table.
UART PrimeCell Identification 2
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | CID2 | ||||||||||||||||||||||||||||||
R-0h | R-5h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CID2 | R | 5h | UART PrimeCell ID Register [23:16] Provides software a standard cross-peripheral identification system. Reset type: PER.RESET |
UARTPCellID3 is shown in Figure 48-32 and described in Table 48-32.
Return to the Summary Table.
UART PrimeCell Identification 3
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | CID3 | ||||||||||||||||||||||||||||||
R-0h | R-B1h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-8 | RESERVED | R | 0h | Reserved |
7-0 | CID3 | R | B1h | UART PrimeCell ID Register [31:24] Provides software a standard cross-peripheral identification system. Reset type: PER.RESET |