SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
FILE: fsi_ex4_loopback_epwmtrigger.c
FSI frame transfer can be triggered by external sources. It can connect up to 32 trigger sources but as of now, only 16 ePWMx-SOCy(x-1:8, y-A:B) are supported. FSI supports external trigger for both PING and DATA frame transfers and in this example we demonstrate how to setup infinite DATA transfers using selectable ePWM-SOC as a trigger source. The TB counter for ePWM operation is in up/down count mode for this example.
Automatic(Hw triggered) Ping frame transmission is also setup along with data.
If there are any comparison failures during transfers or any of error event occurs, execution will stop.
External Connections
For FSI internal loopback (EXTERNAL_FSI_ENABLE == 0), no external connections needed
For FSI external loopback (EXTERNAL_FSI_ENABLE == 1), external connections are required. The FSI TX pins should be connected to the respective FSI RX pins of the same device. See below for external connections to include and GPIOs used:
External Connections Required between FSI TX and RX of the same device:
GPIO_27 -> FSITXA_CLK
Watch Variables