SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Bit | Name | Description |
---|---|---|
31-0 | BUF2AP | Buffer 2 or Buffer 1 Address Pointer |
This bit indicates the physical address of Buffer 2 when a descriptor ring structure is used. There is no limitation for the buffer address alignment. | ||
In 40- or 48-bit addressing mode, these bits indicate the most-significant 8- or 16- bits of the Buffer 1 Address Pointer. |