SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Multiple reset sources of ESCSS are combined to make the reset vector that drives the EtherCAT and companion devices (PHYs) on this MCU. The RESET_OUT is asserted only when configured to be a reset. If configured as an interrupt or NMI, the local host completes the reset.
By default, RESET_OUT performs no action and must be setup to cause the reset to the EtherCAT core and PHY. The input events to RESET_OUT include the remote EtherCAT master, local host application, and EtherCAT soft reset.
When the intent is to perform a reset to the ESCSS and the device, the following options are available to reset the device after software has given a reset to the ESCSS: