SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The ESC RAM has parity logic to make sure the data integrity of the contents. The byte-wide parity is implemented, as PDI accesses to RAM can be done byte wide. To make sure that errors in parity logic itself do not mask the memory error, redundant parity generation logic is used. The parity generated by both logics is compared to make sure safe operation of the memory accesses. Use the INITIATE_MEM_INIT bit from the ESCSS register to trigger the memory initialization.