SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The PWM Sync-chain on the MCU can be triggered either by the device external inputs from the GPIO via input cross-bar or the PWM internal events when the chain is programmed appropriately. The SYNC0/1 inputs in this implementation also act as the external sync inputs to the PWM sync-chain. The integration is shown in Figure 31-18.
The additional select register added to the trigger crossbar register allows independent programming of the EXTSYNCx from either GPTRIP or SYNC0/1.