SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The magic packet contains a unique pattern at any offset after the Destination address, Source address, and Length/Type fields. In addition to the unique pattern matching, the MAC receiver also checks for the following, to detect the received packet as a valid magic packet:
The content of the unique pattern in magic packet is:
If the MAC address of a node is 48'h 00_11_22_33_44_55, the MAC scans for the following data sequence:
Destination Address Source Address Length/Type……………… FF FF FF FF FF FF00 11 22
33 44 55 00 11 22 33 44 55 00 11 22 33 44 55 00 11 22 33 44 5500 11 22 33 44 55
00 11 22 33 44 55 00 11 22 33 44 55 00 11 22 33 44 5500 11 22 33 44 55 00 11 22
33 44 55 00 11 22 33 44 55 00 11 22 33 44 5500 11 22 33 44 55 00 11 22 33 44 55
00 11 22 33 44 55 00 11 22 33 44 55…CRC