SPRUII0F May 2019 – June 2024 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
Bit | Name | Description |
---|---|---|
31-16 | IVT | Inner VLAN Tag |
This field contains the Inner VLAN tag of the received packet if the RS0V bit of RDES3 is set. This is valid only when Double VLAN tag processing and VLAN tag stripping are enabled. | ||
15-0 | OVT | Outer VLAN Tag |
This field contains the Outer VLAN tag of the received packet if the RS0V bit of RDES3 is set. |