This document provides detailed information about various video-input options, user configuration details, and GPIO selection, to make more effective use and yield the targeted benefits of the Fusion application board, from the user's point of view.
MSP430 is a registered trademark of Texas Instruments.
All other trademarks are the property of their respective owners.
The Fusion application board allows up to eight, high-speed, data sources, such as megapixel imagers and RADAR and LIDAR sensors, to be combined into two digital MIPI CSI-2 output ports, which are then connected to a Texas Instruments compatible evaluation module (EVM), with stand-alone operation (see Figure 1). Each sensor source connects to one of the hubs through a single coax cable or twisted pair (HSD). Two DS90UB960 FPD-Link III hubs are on the board. Each DS90UB960 device outputs four, high-speed, data inputs on only one CSI-2 LVDS interface. This greatly simplifies the system by combining eight sensor inputs into two outputs. These outputs are available on an external connector that attaches to an EVM or a similar SoC/processor. Because the Fusion application board supports multiple video inputs and multiplexing options, it is a well suited solution for Advanced Driver Assistance Systems (ADAS) development activity.
The Fusion application board EVM consists of the following:
Use this board with the Texas Instruments compatible EVM to enable a complete system solution.