SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The Destination Read Data FIFO provides a read command translation scoreboard and also stores read data phases that are passing through the RINGACC towards the originating DMA controller. The write interface of the Destination Read Data FIFO is directly connected to the destination VBUSM read data interface. As read data passes through the Destination Read Data FIFO, the rid and rrouteid are changed back to their original values using information which was stored in read command translation scoreboard.