SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
SerDes'es goal is to convert device (SoC) parallel data into serialized data that can be output over a high-speed electrical interface. In the opposite direction, SerDes converts high-speed serial data into parallel data that can be processed by the device. To this end, the SerDes contains a variety of functional blocks to handle both the external analog interface as well as the internal digital logic.
Most important building blocks of SerDes are:
The device contains these SerDeses:
Module Instance | Domain | |
MCU | MAIN | |
SERDES0 | - | ✓ |
Figure 12-1276 shows SERDES0 highlights.