SPRUIM2H May 2020 – October 2023 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The following features are not supported by the module:
Does not support proxy thread sharing. Each host or task must use its own proxy thread within the module if they can access simultaneously or independently. This includes when the task can be interrupted by another task that also uses the proxy
In the system, a proxy must be the only method to access messages that use the same set of queues (to keep credits local), which means all hosts using the same set of message queues must also use the same proxy IP for access and not local proxys
Does not support multiple proxy threads reading from the same queue. For tracking purposes, there can be only 1 consumer proxy thread per queue