SPRUIM6A October 2018 – November 2020
The common processor card has LEDs to indicate the status of the Ethernet link. Some of the LEDs on the CP board are used for industrial applications; those can be controlled with I2C0 of the processor, which is connected to an I/O expander and some processor GPOs.
From the Ethernet PHY, LED1 and GPIO0 are connected to dual LEDs of RJ45 to indicate a 10/100-Mb or 1000-Mb link. The green LED indicates 10/100-Mb speed, and the orange LED indicates 1000-Mb speed.
LED2 is connected to RJ45 LED (Yellow) to indicate transmit/receive activity.