SPRUIM6A October 2018 – November 2020
The addition of the 2.0 revision version of the AM65 EVM required a few changes. The initial voltage of the VDD_CORE supply was changed to 1.1 V from 1.0 V for earlier versions of the silicon. The MMC0 SDCD, MMC0_SDWP, MMC1_SDCD, and MMC1_SDWP were moved to a different IO bank in 2.0 revision, so the source voltage for the signals driving these pins was updated. 49.9K pull-up resistors for MMC0_DAT0-7 and MMC0_CLK signals. For more information about these changes, review the Silicon Errata document.