SPRUIN7C March 2020 – March 2024 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
FILE: hic_ex1_config_16bit.c
Example sets up Host Interface Controller Module in 16-bit mode the data memory of device is accessed by the External Host.
This example is validated on an TI Internal Validation Platform will not run in F28002x Control Card The example initializes the GPIOs for 16 bit Memory access mode with separate Read and Write Control Pins, Extended Wait, and nRDY pin The example demonstrates the following sequences
External Connections
This is tested on TI Internal validation platform hence no connection needed on Control card. This has been tested with F2838x EMIF interface.
Watch Variables
None