This user's guide describes the structure and use of the Configurable Logic Block (CLB) tool. It is assumed that the reader is already familiar with the architecture of the CLB and with the CCS IDE. Information on the architecture of the CLB may be found in the device-specific technical reference manual (TRM).
C2000™ and Code Composer Studio™ are trademarks of Texas Instruments.
All trademarks are the property of their respective owners.
The CLB is a hardware module integrated into certain C2000™ devices. The CLB contains a set of configurable blocks and inter-connections which allows users to create their own custom digital logic along the lines of what could be done with an FPGA. The CLB can enhance the functionality of existing device peripherals or create new peripheral functions. There are different versions of the CLB which have been released for devices in the past. Refer to the C2000 Real-Time Control MCU Peripherals for more information on what CLB type is available for a certain device. The CLB is configured using a software utility, referred to here as the CLB tool.
The CLB tool allows the user to configure and connect sub-modules in each CLB tile. The tool is included under the name Tile Design within the SysConfig graphical user interface (GUI) which is part of Code Composer Studio™ (CCS). The tool includes examples intended to help the user explore the features of the tool and create their own projects.
The tool generates a C header file containing a set of constants corresponding to the configuration settings defined by the user in the GUI. The tool also generates a C source file which uses the constants in the C header file to initialize the CLB modules by loading the constants into the CLB registers by a sequence of register load operations. The functions in the C source file must be called during the device initialization. To configure the input and output connections between the CLB tile and other device peripherals, including the cross-bars and other CLB tiles, use the CLB module within SysConfig. The configuration of these connections must be done separately from the CLB tool. The CLB tool includes the capability for simulating these inputs and testing the functionality of the tile configuration.
The CLB tool is based on the SysConfig tool in CCS. The generated C header and source files, combined with the C2000Ware SDK, can configure the CLB. To conduct a simulation of the design a number of third party tools need to be installed, including a compiler and a wave viewer. For more information on the CLB simulator, see Section 3.5.
The CLB tool generates a “.dot” file which shows sub-module inter-connections in diagram form and can help verify the design. This file is created in HTML and SVG formats using CCS post-build steps. These steps use node.js and JavaScript libraries which are in the provided examples. The tool also generates a “clb_sim.cpp” file. The CPP file, along with other CLB simulation models, is compiled using a GCC compiler. The output of the compilation is an “.exe” file, which must be executed on the local machine in order to generate a “.vcd” file. This “.vcd” file can be used to conduct a timing analysis using an external graph viewer. All these steps are done by the "clb_simulation" file which is generated by the tool. This file will be either a batch (.bat) or shell (.sh) file depending on the operating system used (the images used in this user's guide are based on the Windows operating system). This file must be executed to generate the appropriate ".vcd" file.
The CLB configuration is encoded in the generated C header file “clb_config.h”. The “clb_config.c” file generated by the CLB tool uses the generated header file to load the configuration into the CLB module’s registers. The CLB module within SysConfig must have the appropriate Tile Design attached for the configuration to actually take place, as shown in Figure 1-1. The independence between Tile Designs and the CLB module in SysConfig allows any number of tile configurations to be created while having a limited number of CLB instances on a device. These Tile Designs are selectively loaded into the CLB.
It is important to note that in the application code for the C28x device, the functions in the “clb_config.c” file must be called during the device initialization steps. Figure 1-2 shows the output of the CLB tool and the post-build steps.
In a typical scenario, the user begins by specifying the CLB logic functionality. This may be in the form of a logic circuit diagram, timing information, written description, VHDL code, or some other form. Having installed the requisite tools, the first step will be to connect the tile sub-modules to implement the desired logic.
The specification may include a set of timing diagrams in which case the user may choose to conduct a simulation of the CLB configuration to ensure behavior is as expected. This step includes defining a set of input test stimuli and building a simulation project to generate simulation waveforms which can be opened in a graph viewer. If the results are not as expected, the user can modify the CLB tool settings and repeat the simulation.
Once the simulation produces the correct waveform, the user can download the design into the device using CCS to run or debug the code.
In a CCS project with SysConfig enabled for a C28x device, the steps to create the HTML and SVG block diagram of the Tile Designs is done as part of the post-build steps. When the user builds the CCS project, the user application code and the generated “clb_config.h” and “clb_config.c” are compiled using the C28x compilers and a “.out” file is generated.
The "clb_simulation" file compiles the generated simulation files, “clb_sim.cpp” and “clb_config.h”, and the CLB simulation modes using a GCC compiler. The output of this step is a “.exe” file (“simulation_output.exe”) which is automatically run to generate the “CLB.vcd” file. This file can be viewed using an external graph viewer.
In CLB Tool Build Process the BUILD_CONFIG_LOC directory is the directory used as the build configuration output for the project (this can be "Debug", "CPU1_RAM", and so forth), and shares the name of the active build configuration.