SPRUIR8B april 2020 – july 2023
The top panel in the configuration tool contains “Global Parameters” settings used in simulation. Click the '?' icon to see a short description.
The "Generate CLB Simulation File" is used to generate the content of the "clb_simulation" file. This file, when executed, will generate the .vcd for all of the CLB Tile Designs. This .vcd file will appear in the directory above where the batch file is executed, within a newly created "simulation" directory.
The “Clock Period (ps)” is the period of the CLB clock in picoseconds used for simulation purposes. The “Simulation Duration (ps)” field allows users to control the duration of the simulation run in picoseconds. The “Reset Duration (ps)” field allows the user to insert a delay in picoseconds to mimic the effect of a device reset.