SPRUIR8B april 2020 – july 2023
The CLB is a hardware module integrated into certain C2000™ devices. The CLB contains a set of configurable blocks and inter-connections which allows users to create their own custom digital logic along the lines of what could be done with an FPGA. The CLB can enhance the functionality of existing device peripherals or create new peripheral functions. There are different versions of the CLB which have been released for devices in the past. Refer to the C2000 Real-Time Control MCU Peripherals for more information on what CLB type is available for a certain device. The CLB is configured using a software utility, referred to here as the CLB tool.