SPRUIS4E March 2022 – January 2024
The default configuration of the DP83867 is determined using a number of resistor pull-up and pull-down values on specific pins of the PHY. Depending on the values installed each of the configuration pins can be set to one of four modes by using the pull up and pull down options provided. The EVM uses the 48-pin QFN package, designated with the RGZ suffix, which supports only RGMII interface.
The DP83867 PHY uses four level configurations based on resistor strapping that generate four distinct voltages ranges. The resistors are connected to the RX data and control pins that are normally driven by the PHY and are inputs to the processor. The voltage range for each mode is shown below:
These are the defaults set for the MCU RGMII.
The strapping resistors are shown in Figure 4-16.