SPRUIS4E March 2022 – January 2024
The EVM supports multiple User Push buttons for providing Reset inputs and User Interrupts to the processor.
Table 3-5 lists the Push buttons that are placed on the Top side of the Common Processor Board.
Sl No | Push Buttons | Signal | Function |
---|---|---|---|
1 | SW7 | MCU_PORz | MCU domain Power on Reset input |
2 | SW5 | MCU_RESETz | MCU domain Warm Reset input |
3 | SW4 | PORz | Main domain Power on Reset input |
4 | SW6 | RESET_REQz | Main domain Warm Reset input |
5 | SW10 | SOC_EXTINTn | External Interrupt input |
6 | SW11 | SYS_IRQz | System IRQ Interrupt input (also used as SYS_WAKE) |
7 | SW12 | MCAN0_WAKE | CAN Wakeup Input |