SPRUIS8A january   2020  – august 2023 DRA829J , DRA829J-Q1 , DRA829V , DRA829V-Q1 , TDA4VM , TDA4VM-Q1

 

  1.   1
  2.   Trademarks
  3. 1Introduction
  4. 2Step 1: Setup EVM and Expansion Card Hardware
    1. 2.1 Attaching the SOM to the Common Processor Board
    2. 2.2 Attaching an Optional Expansion Card
  5. 3Step 2: Experiencing the Out Of Box (OOB) Demonstration to Ensure the EVM Hardware is Functional
  6. 4Step 3: Download and Install Processor SDK (softweare development kit)
  7. 5Step 4: Project 0, Your First ‘Hello World’ project to Ensure Interoperability of EVM and Software
  8.   Additional Resources
  9.   A Installing the Automotive Gateway/Ethernet Switch/Industrial Expansion Card Onto the Common Processor Board
  10.   B Installing the Infotainment Expansion Board Onto the Common Processor Board
  11.   Revision History

Installing the Infotainment Expansion Board Onto the Common Processor Board

  1. Remove the stand-offs (8x) from the EVM. Mate the Infotainment Expansion Board onto the common processor board expansion connectors (see Figure 7-1 left).
  2. Press firmly on the edges to ensure the connectors mate (may have to apply significant pressure).
  3. If a CSI expansion board is not connected to the CSI expansion connectors on the common processor board, add a 2mm thick washer to each of the four stand-offs (see Figure 7-1 right) on the common processor board. Washers are included in the kit.
  4. Re-install the eight stand-offs.
GUID-20230728-SS0I-N8ZJ-QPVJ-H5PKQQSGVQMS-low.png Figure B-1 Installing the Infotainment Expansion Board Onto the Common Processor Board