SPRUIT5 April 2021 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
The various redundancy architectures possible for the safety instrumented systems are indicated in Table 8-1. For more information, see [10].
Diagnostic Implementation | ||
---|---|---|
1 | 1oo1 Architecture![]() |
None. |
2 | 1oo1D![]() |
Diagnostic channel is implemented using various hardware diagnostic features like Watchdog, and so forth. |
3 | 1oo2![]() |
Two different processing units are used to implement one channel. |
4 | 2oo2![]() |
Two different processing units are used to implement one channel. |
5 | 2oo2D![]() |
Two 1oo1D structures of #2 wired together to implement a safe channel. |
6 | 2oo2D Same figure as above. |
Two 1oo1D structures of #3 wired together. |
7 | 1oo2D![]() |
Similar to 2oo2D implementation of #6 with additional control lines wired to control one set of units using the other unit |
8 | 1oo2D Same figure as above. |
Similar to 2oo2D implementation of #7 with additional control lines wired to control one set of units using the other unit. |
9 | 2oo3![]() |
Use three different processing units to implement majority voting. The fourth channel can be used either standalone or with hardware diagnostic features. |