SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
Resets bring the device or part of the device to a known state after events such as power-up or hardware or software requests.
Figure 5-751 shows an overview of the reset architecture.
For power modules used in the reset see:
For information about Boot modes and Boot configuration pins, see Initialization.
MOD_POR_RST[n] and MOD_G_RST[n] are connected to certain modules. For more information which is the number of the LPSC of a certain module, see its specific chapter.