All ports
The total number of transmit frames on the port that had a memory protect CRC error on egress:
- Any frame destined to be transmitted,
- Was any size
- Had a memory protect CRC error on egress.
Note: - Frames to the host with memory protect errors are dropped via TXST_DROP. Ethernet frames will have at least one byte of the generated port type CRC inverted on egress.
- This statistic is 8-bits wide only and will not rollover but will limit at 0xFF.
- A non-zero value in this statistic will issue a STAT_PEND0 interrupt for the associated port.