SPRUIU1C July 2020 – February 2024 DRA821U , DRA821U-Q1
Each time an event message is received on the Main Event Transport Lane interface, the interrupt mapping block performs a direct lookup into an SRAM using the event number as the address. The SRAM stores a corresponding raw interrupt status register and bit number within that register which are to be manipulated anytime a message is received indicating something occurred on that specific event. When an up event is received, the specified bit in the j Status register will be set. When a down event is received, that same bit will be cleared. This block is what allows flexible aggregation of various system events into an array of bits in the interrupt status registers. It is intended that this mapping is essentially static - set up when a resource is allocated and left untouched until the resource is no longer needed. Note that the 'cnt' field of the ETL is ignored and no interrupt counting is performed here. When 'UpDn=1', the interrupt flag bit is set, and when 'UpDn=0', the flag bit is cleared.