KeyStone is a trademark of Texas Instruments.
Arm is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
Wi-Fi is a registered trademark of Wi-Fi Alliance.
All trademarks are the property of their respective owners.
The Jacinto7 J7200 (DRA821) EVM is a standalone test, development, and evaluation module system that enables developers to write software and develop hardware around Jacinto7 J7200 (DRA821) processor subsystem. The J7200 processor is a KeyStone™ III-based Multicore Arm® System-on-Chip (SoC).
The processor/device may be available in different configurations targeted for specific markets. This EVM will support development of the super-set device (J7200) as well as the market specific devices (DRA821). Many features of the J7200 system are available on the EVM, which gives developers the basic resources needed for most general-purpose type.
The J7200 EVM is comprised of :
J7200 EVM has been designed to enable customers to evaluate the Processor’s performance with flexibility. For the flexibility, different interface/expansion boards have been designed. Some examples include:
The J7200 EVM is a high performance, standalone development platform that enables users to evaluate the Texas Instrument’s Keystone III System-on-Chip (SoC).
Below are the EVM’s key features