SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Flash read or instruction fetch accesses can be classified either as a Flash access (access to an address location in Flash), or an OTP access (access to an address location in OTP).
When the CPU performs an access to a Flash memory address, data is returned after (RWAIT+1) SYSCLK cycles.
For a USER-OTP access, data is returned after 11 SYSCLK cycles.
RWAIT defines the number of random access wait states, and is configured using the RWAIT field in the FRDCNTL register. At reset, RWAIT defaults to a worst-case wait state count (15), and therefore must be initialized to the appropriate number of wait states to improve performance, based on the CPU clock frequency and the access time of the Flash. The Flash supports zero-wait accesses when RWAIT is set to zero, when the CPU clock frequency is low enough to accommodate the Flash access time.
For a given system clock frequency, configure RWAIT using the following formula:
For C28x Flash Bank: RWAIT = ceiling[(SYSCLK/FCLK)-1]
where SYSCLK is the system operating frequency for CPU1, and FCLK is the clock frequency for Flash.
FCLK must be ≤ FCLKmax, the allowed maximum Flash clock frequency at RWAIT=0.
If RWAIT results in a fractional value when calculated using the above formula, round up RWAIT to the nearest integer.