SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Table 3-286 lists the memory-mapped registers for the SYNC_SOC_REGS registers. All register offset addresses not listed in Table 3-286 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Write Protection | Section |
---|---|---|---|---|
0h | SYNCSELECT | Sync Input and Output Select Register | EALLOW | Go |
2h | ADCSOCOUTSELECT | External ADCSOC Select Register | EALLOW | Go |
4h | SYNCSOCLOCK | SYNCSEL and EXTADCSOC Select Lock register | EALLOW | Go |
Complex bit access types are encoded to fit into small table cells. Table 3-287 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
R-0 | R -0 | Read Returns 0s |
Write Type | ||
W | W | Write |
WSonce | W Sonce | Write Set once |
Reset or Default Value | ||
-n | Value after reset or the default value | |
Register Array Variables | ||
i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. |
SYNCSELECT is shown in Figure 3-266 and described in Table 3-288.
Return to the Summary Table.
Sync Input and Output Select Register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | SYNCOUT | ||||||
R/W-7h | R/W-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | RESERVED | ||||||
R-0-0h | R/W-7h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | RESERVED | RESERVED | RESERVED | ||||
R/W-7h | R/W-7h | R/W-7h | R/W-7h | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | RESERVED | RESERVED | |||||
R/W-7h | R/W-7h | R/W-7h | |||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-29 | RESERVED | R/W | 7h | Reserved |
28-24 | SYNCOUT | R/W | 0h | Select Syncout Source: 00000: EPWM1SYNCOUT selected to drive the SYNCOUT pin. 00001: EPWM2SYNCOUT selected to drive the SYNCOUT pin. 00010: EPWM3SYNCOUT selected to drive the SYNCOUT pin. 00011: EPWM4SYNCOUT selected to drive the SYNCOUT pin. 00100: EPWM5SYNCOUT selected to drive the SYNCOUT pin. 00101: EPWM6SYNCOUT selected to drive the SYNCOUT pin. 00110: EPWM7SYNCOUT selected to drive the SYNCOUT pin. 00111: EPWM8SYNCOUT selected to drive the SYNCOUT pin. 01000: Reserved 01001: Reserved 01010: Reserved 01011: Reserved 01100: Reserved 01101: Reserved 01110: Reserved 01111: Reserved 10000: Reserved 10001: Reserved 10010: Reserved 10011: Reserved 10100: Reserved 10101: Reserved 10110: Reserved 10111: Reserved 11000: ECAP1SYNCOUT selected to drive the SYNCOUT pin. 11001: ECAP2SYNCOUT selected to drive the SYNCOUT pin. 11010: ECAP3SYNCOUT selected to drive the SYNCOUT pin. 11011: Reserved 11100: Reserved 11101: Reserved 11110: Reserved 11111: Reserved Notes: [1] Reserved position defaults to 00 selection Reset type: SYSRSn |
23-18 | RESERVED | R-0 | 0h | Reserved |
17-15 | RESERVED | R/W | 7h | Reserved |
14-12 | RESERVED | R/W | 7h | Reserved |
11-9 | RESERVED | R/W | 7h | Reserved |
8-6 | RESERVED | R/W | 7h | Reserved |
5-3 | RESERVED | R/W | 7h | Reserved |
2-0 | RESERVED | R/W | 7h | Reserved |
ADCSOCOUTSELECT is shown in Figure 3-267 and described in Table 3-289.
Return to the Summary Table.
External ADCSOC Select Register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | |||
R-0-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
PWM8SOCBEN | PWM7SOCBEN | PWM6SOCBEN | PWM5SOCBEN | PWM4SOCBEN | PWM3SOCBEN | PWM2SOCBEN | PWM1SOCBEN |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | RESERVED | RESERVED | RESERVED | RESERVED | |||
R-0-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
PWM8SOCAEN | PWM7SOCAEN | PWM6SOCAEN | PWM5SOCAEN | PWM4SOCAEN | PWM3SOCAEN | PWM2SOCAEN | PWM1SOCAEN |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-28 | RESERVED | R-0 | 0h | Reserved |
27 | RESERVED | R/W | 0h | Reserved |
26 | RESERVED | R/W | 0h | Reserved |
25 | RESERVED | R/W | 0h | Reserved |
24 | RESERVED | R/W | 0h | Reserved |
23 | PWM8SOCBEN | R/W | 0h | ADCSOCBOn source select: 0: Respective EPWM SOCB output is not selected 1: Respective EPWM SOCB output is selected Reset type: SYSRSn |
22 | PWM7SOCBEN | R/W | 0h | ADCSOCBOn source select: 0: Respective EPWM SOCB output is not selected 1: Respective EPWM SOCB output is selected Reset type: SYSRSn |
21 | PWM6SOCBEN | R/W | 0h | ADCSOCBOn source select: 0: Respective EPWM SOCB output is not selected 1: Respective EPWM SOCB output is selected Reset type: SYSRSn |
20 | PWM5SOCBEN | R/W | 0h | ADCSOCBOn source select: 0: Respective EPWM SOCB output is not selected 1: Respective EPWM SOCB output is selected Reset type: SYSRSn |
19 | PWM4SOCBEN | R/W | 0h | ADCSOCBOn source select: 0: Respective EPWM SOCB output is not selected 1: Respective EPWM SOCB output is selected Reset type: SYSRSn |
18 | PWM3SOCBEN | R/W | 0h | ADCSOCBOn source select: 0: Respective EPWM SOCB output is not selected 1: Respective EPWM SOCB output is selected Reset type: SYSRSn |
17 | PWM2SOCBEN | R/W | 0h | ADCSOCBOn source select: 0: Respective EPWM SOCB output is not selected 1: Respective EPWM SOCB output is selected Reset type: SYSRSn |
16 | PWM1SOCBEN | R/W | 0h | ADCSOCBOn source select: 0: Respective EPWM SOCB output is not selected 1: Respective EPWM SOCB output is selected Reset type: SYSRSn |
15-12 | RESERVED | R-0 | 0h | Reserved |
11 | RESERVED | R/W | 0h | Reserved |
10 | RESERVED | R/W | 0h | Reserved |
9 | RESERVED | R/W | 0h | Reserved |
8 | RESERVED | R/W | 0h | Reserved |
7 | PWM8SOCAEN | R/W | 0h | ADCSOCAOn source select: 0: Respective EPWM SOCA output is not selected 1: Respective EPWM SOCA output is selected Reset type: SYSRSn |
6 | PWM7SOCAEN | R/W | 0h | ADCSOCAOn source select: 0: Respective EPWM SOCA output is not selected 1: Respective EPWM SOCA output is selected Reset type: SYSRSn |
5 | PWM6SOCAEN | R/W | 0h | ADCSOCAOn source select: 0: Respective EPWM SOCA output is not selected 1: Respective EPWM SOCA output is selected Reset type: SYSRSn |
4 | PWM5SOCAEN | R/W | 0h | ADCSOCAOn source select: 0: Respective EPWM SOCA output is not selected 1: Respective EPWM SOCA output is selected Reset type: SYSRSn |
3 | PWM4SOCAEN | R/W | 0h | ADCSOCAOn source select: 0: Respective EPWM SOCA output is not selected 1: Respective EPWM SOCA output is selected Reset type: SYSRSn |
2 | PWM3SOCAEN | R/W | 0h | ADCSOCAOn source select: 0: Respective EPWM SOCA output is not selected 1: Respective EPWM SOCA output is selected Reset type: SYSRSn |
1 | PWM2SOCAEN | R/W | 0h | ADCSOCAOn source select: 0: Respective EPWM SOCA output is not selected 1: Respective EPWM SOCA output is selected Reset type: SYSRSn |
0 | PWM1SOCAEN | R/W | 0h | ADCSOCAOn source select: 0: Respective EPWM SOCA output is not selected 1: Respective EPWM SOCA output is selected Reset type: SYSRSn |
SYNCSOCLOCK is shown in Figure 3-268 and described in Table 3-290.
Return to the Summary Table.
SYNCSEL and EXTADCSOC Select Lock register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | ADCSOCOUTSELECT | SYNCSELECT | |||||
R-0-0h | R/WSonce-0h | R/WSonce-0h | |||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-2 | RESERVED | R-0 | 0h | Reserved |
1 | ADCSOCOUTSELECT | R/WSonce | 0h | ADCSOCOUTSELECT Register Lock bit: 0: Respective register is not locked 1: Respective register is locked. Notes: [1] Any bit in this register, once set can only be creaed through a SYSRSn. Write of 0 to any bit of this regtister has no effect [2] The locking mechanism applies to only writes. Reads to the registers which have LOCK protection are always allowed Reset type: SYSRSn |
0 | SYNCSELECT | R/WSonce | 0h | SYNCSELECT Register Lock bit: 0: Respective register is not locked 1: Respective register is locked. Notes: [1] Any bit in this register, once set can only be creaed through a SYSRSn. Write of 0 to any bit of this regtister has no effect [2] The locking mechanism applies to only writes. Reads to the registers which have LOCK protection are always allowed Reset type: SYSRSn |