SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
FILE: can_ex4_loopback_dma.c
This example sets up the CAN module to transmit and receive messages on the CAN bus. The CAN module is set to transmit a 4 byte message internally. An interrupt is used to assert the DMA request line which then triggers the DMA to transfer the received data from the CAN interface register to the receive buffer array. A data check is performed once the transfer is complete.
This example sets up the CAN controller in External Loopback test mode. Data transmitted is visible on the CANTXA pin and is received internally back to the CAN Core. Please refer to details of the External Loopback Test Mode in the CAN Chapter in the Technical Reference Manual. Please refer to the appnote Programming Examples and Debug Strategies for the DCAN Module (www.ti.com/lit/SPRACE5) for useful information about this example
External Connections
Watch Variables