SPRUIW9C October 2021 – March 2024 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Data consistency is provided by indirect accesses to the message objects. During normal operation, all CPU and DMA accesses to the message RAM are done through Interface registers. The IFx registers can be thought of as a "window" through which the message objects (mailboxes) are accessed.
Three Interface register sets control the CPU read and write accesses to the Message RAM, see Figure 28-2. There are two Interface register sets for read/write access (IF1 and IF2) and one Interface register set for read access only (IF3). See also Section 28.13. The Interface registers have the same word length as the message RAM.
In a dedicated test mode, the message RAM is memory-mapped and can be directly accessed.