SPRUIX1B October 2022 – April 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
The software library function SFO(), calculates the MEP scale factor for the HRPWM-supported ePWM modules. The scale factor is an integer value in the range 1-255, and represents the number of micro step edge positions available for a system clock period. The scale factor value is returned in an integer variable called MEP_ScaleFactor. For example, see Table 13-20.
Software Function call | Functional Description | Updated Variables |
---|---|---|
SFO() | Returns MEP scale factor in the HRMSTEP register | MEP_ScaleFactor and HRMSTEP register. |
To use the HRPWM feature of the ePWMs, it is recommended that the SFO function be used as described here.
Step 1. Add "Include" Files
The SFO_V8.h file needs to be included as follows. This include file is mandatory while using the SFO library function. For the SFO() to operate, the appropriate (Device)_Device.h and (Device)_Epwm_defines.h must be included in the project. These include files are optional if customized header files are used in the end applications.