Once the application requirements are
understood, a specific clock configuration can be determined. The default
configuration is for INTOSC2 to be used as the system clock (PLLSYSCLK) with a
divider of 1. The following procedure can be used to set up the desired application
configuration:
Refer to your device SysCtl_setClock()
function inside C2000Ware installation for an example.
Recommended sequence to set up the
system PLL:
- Bypass the PLL by clearing
SYSPLLCTL1[PLLCLKEN]. Allow at least 60 NOP instructions for this to take
effect.
- Power down the PLL by writing to SYSPLLCTL1.PLLEN = 0 and allow
at least 60 NOP instructions for this to take effect.
- Select the reference clock source (OSCCLK) by writing to
CLKSRCCTL1.OSCCLKSRCSEL. Allow at least 300 NOP instructions for this to take
effect.
- Set the system clock divider to
/1 to make sure the fastest PLL configuration by clearing SYSCLKDIVSEL[
PLLSYSCLKDIV].
- Set the IMULT, REFDIV, and ODIV
simultaneously by writing 32-bit value in SYSPLLMULT at once. This automatically
enables the PLL. Be sure the settings for the multiplier and dividers do not
violate the frequency specifications as defined in the TMS320F280013x
Real-Time Microcontrollers Data Sheet .
- Wait for PLL to lock by polling
for lock status bit to go high (SYSPLLSTS.LOCKS = 1).
- Configure DCC with reference clock as OSCCLK and clock under
measurement as PLLRAWCLK, and verify the frequency of the PLL. If the frequency
is out of range, do not enable PLLRAWCLK as SYSCLK, stop here and troubleshoot.
Refer to Chapter 7 for more information on the configuration and usage.
- Switch to the PLL as the system clock by setting
SYSPLLCTL1[PLLCLKEN].
Note:
- SYSPLL must be bypassed and powered down manually before
changing the OSCCLK source.
- At least 60 CPU clock cycles delay is needed after
bypassing PLL, that is, SYSPLLCTL1.PLLCLKEN = 0.
- At least 60 CPU clock cycles delay is needed after PLL is
powered down, that is, SYSPLLCTL1.PLLEN = 0.
- At least 300 CPU clock cycles delay is needed after
OSSCLK source is changed.
- PLL SLIP bit is not supported. DCC can be used to check
the validity of the PLL clock. This feature is included as part of
SysCtl_setClock() function inside C2000Ware.