SPRUIX1B October 2022 – April 2024 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
If the application requires the PLL clock to be bypassed from the system, then the application needs to configure SYSPLLCTL1.PLLCLKEN = 0. It takes up to 60 CPU clock cycles before the bypass is effective. In the meantime if PLLSYSCLKDIV is reduced to a lower value (for example from /2 to /1, /4 to /2, and so on), the device can be clocked above the maximum rated frequency and can lead to unpredictable device behavior. Hence, a delay of 60 CPU clock cycles is required after bypassing the PLL from the enable state, that is, going from PLLCLKEN = 1 to PLLCLKEN = 0.