SPRUIY5A February 2021 – July 2021 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6422 , AM6441 , AM6442
The middle priority interfaces and the power distribution planes and pours are routed after the SERDES and DDR interfaces. TI strongly recommends completing all SERDES and DDR routing before continuing with other interfaces. Note that the power distribution planes and pours and all of the decoupling must be placed before PCB simulations are executed for the SERDES and DDR routes. TI strongly recommends that simulation be performed on the higher speed source-synchronous interfaces, such as RGMII, OSPI, and QSPI. Routing for these interfaces should be completed at this time.
Special care is needed for the 3.3 μF output capacitor connected to the CAP_VDDSHV_MMC1 pin on the SoC. This capacitor should be placed as close to the pin as possible and a low inductance path should be present between the CAP_VDDSHV_MMC1 output and the VDDSHV5 voltage pins for the MMC1 IO voltage. This allows the internal LDO to generate either the 3.3 V or 1.8 V needed for an SD Card. The layout used on the AM64 GP EVM is shown in Figure 7-1.
This placement can be improved if the capacitor can be placed directly under the SoC. An alternate layout is shown in Figure 7-2.